I'm trying to build an ubuntu image for the s32g399ardb3 using the S32G3 Linux BSP44.0.
I have the machine set to s32g399ardb3ubuntu and running bitbake fsl-image-ubuntu gives an error:
ERROR: Nothing PROVIDES 'virtual/x86_64-fslbsp-linux-gcc-crosssdk' (but /newhome/arthur/fsl-auto-yocto-bsp44.0_s32g/sources/meta-alb/meta-alb-sdk/recipes-devtools/binutils2.34/binutils-cross-canadian_2.34.bb DEPENDS on or otherwise requires it). Close matches:
virtual/x86_64-fslbsp-linux-g++
virtual/x86_64-fslbsp-linux-gcc
virtual/x86_64-fslbsp-linux-go
I can build the fsl-image-auto image in BSP44.0 for s32g399ardb3.
I can also build the fsl-image-ubuntu image in BSP43.0 for s32g399ardb3ubuntu.
The machine I am building on is:
SB Version: core-11.1.0ubuntu2-noarch:printing-11.1.0ubuntu2-noarch:security-11.1.0ubuntu2-noarch
Distributor ID: Ubuntu
Description: Ubuntu 20.04.6 LTS
Release: 20.04
Codename: focal
Kernel version is 5.4.0-204-generic and ldd (Ubuntu GLIBC 2.31-0ubuntu9.18) 2.31
There are log warnings qabout the preferred version of 2.35 of glibc not available.
Am I missing a package?
Regards,
Arthur.
Full log:
arthur@nmgPowerEdgeT630:~/fsl-auto-yocto-bsp44.0_s32g/build_s32g399ardb3ubuntu$ bitbake fsl-image-ubuntu
Loading cache: 100% |##############################################################################################################| Time: 0:00:02
Loaded 5800 entries from dependency cache.
Parsing recipes: 100% |############################################################################################################| Time: 0:00:01
Parsing of 3692 .bb files complete (3691 cached, 1 parsed). 5803 targets, 615 skipped, 2 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
WARNING: preferred version 2.35 of cross-localedef-native not available (for item cross-localedef-native)
WARNING: versions of cross-localedef-native available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-cross-aarch64 not available (for item virtual/aarch64-fsl-linux-binutils)
WARNING: versions of binutils-cross-aarch64 available: 2.34 2.42
WARNING: preferred version 2.35 of cross-localedef-native not available (for item cross-localedef-native)
WARNING: versions of cross-localedef-native available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of cross-localedef-native not available (for item cross-localedef-native-dev)
WARNING: versions of cross-localedef-native available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-crosssdk-x86_64-fslbsp-linux not available (for item virtual/x86_64-fslbsp-linux-binutils)
WARNING: versions of binutils-crosssdk-x86_64-fslbsp-linux available: 2.42
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item virtual/nativesdk-libc)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item virtual/libc)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-native not available (for item binutils-native)
WARNING: versions of binutils-native available: 2.42
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item virtual/nativesdk-libintl)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item virtual/nativesdk-libiconv)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-utils)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-dbg)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-dev)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc-locale not available (for item glibc-localedata-i18n)
WARNING: versions of glibc-locale available: 2.31 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc-thread-db)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.38 of binutils-cross-canadian-aarch64 not available (for item binutils-cross-canadian-aarch64)
WARNING: versions of binutils-cross-canadian-aarch64 available: 2.34 2.42
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-ldconfig)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-glibc-dev)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-glibc)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of nativesdk-glibc not available (for item nativesdk-glibc-utils)
WARNING: versions of nativesdk-glibc available: 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item glibc)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item ldconfig)
WARNING: versions of glibc available: 2.31+git 2.39+git
WARNING: preferred version 2.35 of glibc-locale not available (for item glibc-locale)
WARNING: versions of glibc-locale available: 2.31 2.39+git
WARNING: preferred version 2.35 of glibc not available (for item virtual/libintl)
WARNING: versions of glibc available: 2.31+git 2.39+git
ERROR: Nothing PROVIDES 'virtual/x86_64-fslbsp-linux-gcc-crosssdk' (but /newhome/arthur/fsl-auto-yocto-bsp44.0_s32g/sources/meta-alb/meta-alb-sdk/recipes-devtools/binutils2.34/binutils-cross-canadian_2.34.bb DEPENDS on or otherwise requires it). Close matches:
virtual/x86_64-fslbsp-linux-g++
virtual/x86_64-fslbsp-linux-gcc
virtual/x86_64-fslbsp-linux-go
NOTE: Runtime target 'binutils-cross-canadian-aarch64' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['binutils-cross-canadian-aarch64', 'virtual/x86_64-fslbsp-linux-gcc-crosssdk']
NOTE: Runtime target 'packagegroup-cross-canadian-s32g399ardb3' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['packagegroup-cross-canadian-s32g399ardb3', 'binutils-cross-canadian-aarch64', 'virtual/x86_64-fslbsp-linux-gcc-crosssdk']
ERROR: Required build target 'fsl-image-ubuntu' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-ubuntu', 'packagegroup-cross-canadian-s32g399ardb3', 'binutils-cross-canadian-aarch64', 'virtual/x86_64-fslbsp-linux-gcc-crosssdk']
Summary: There were 48 WARNING messages.
Summary: There were 2 ERROR messages, returning a non-zero exit code.
Linux BSP support no longer includes the Ubuntu rootfs following the migration to Poky 5.0. This limitation is also documented in the Linux BSP Release Notes for BSP version 44.
Apologies this is a duplicate of https://community.nxp.com/t5/AP-Software-Support/Linux-BSP-44-build-errors/td-p/2164327 with possibly a bit more information.
Regards,
Arthur.