2163633_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2163633_en-US

2163633_en-US

PFE on S32G A53 QNX ERROR
 
 
Hi,NXP experts
We have a custom board that we want to run QNX and PFE drivers on. But we have encountered the following problem and would like to ask PFE experts to help analyze it.
 
 
software information:
PFE QNX driver version: 1.8.0
PFE FW version: 1.11.0
QNX SDP version: 7.1.0
BSP version of QNX S32G399A: BSP_nxp-s32g-rdb3_br-710_be-710_SVN996606_JBN10
 
hardware information:
The difference in hardware between us and the NXP S32G399ARDB3 EVN board is that DDR has been changed to 2GB, and we have already adapted it in Linux, and the pfe Ethernet driver is normal.
The changes are as follows:
 
 
 
 
 
1. Changes in images/s32g399a-rdb.build file,
 
SandalWood_0-1756983841389.pngSandalWood_0-1756983841389.png
2. Changes in src\hardware\startup\boards\s32g\s32g399a-rdb\s32g_init_raminfo.c file:
 
SandalWood_1-1756983875619.pngSandalWood_1-1756983875619.png
 
3. Other insignificant changes, unrelated to the PFE driver.
 
 
 
My test commands are:
# slog2info -c  
# slog2info -w &
# io-pkt-v6-hc -p tcpip pkt_typed_mem=pfe_ddr -d /proc/boot/devnp-pfe-2.so class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw
 
However, after running, the error message appears.Log is here.
-------------------Appendix------------------
 
 
NOTICE:  The list of clocks found enabled during the SCMI agent reset command:
NOTICE:         linflex_lin
NOTICE:         usdhc_core
board_smp_num_cpu: 8 cores
MMU: 16-bit ASID 40-bit PA TCR_EL1=b5183519
ARM GIC-500 r1p1, arch v3.0 detected
board_smp_num_cpu: 8 cores
board_smp_num_cpu: 8 cores
No SPI intrinfo. Add default entry for 32 -> 575 vectors, Ok
cpu0: MPIDR=80000000
cpu0: MIDR=410fd034 Cortex-A53 r0p4
cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu0: L1 Icache 32K linesz=64 set/way=256/2
cpu0: L1 Dcache 32K linesz=64 set/way=128/4
cpu0: L2 Unified 1024K linesz=64 set/way=1024/16
board_smp_num_cpu: 8 cores
 
A53 CORE CLOCK : 1000MHz
DDR CLOCK      : 800MHz
SERDES CLOCK   : 2000MHz
LINFLEXD CLOCK : 125MHz
GMAC TS CLOCK  : 48MHz
SPI CLOCK      : 48MHz
QSPI CLOCK     : 800MHz
SDHC CLOCK     : 800MHz
 
Loading IFS...decompressing...done
board_smp_start: cpu_cluster_id: 0, cpu_id: 1
NOTICE:  S32 TF-A: s32_pwr_domain_on: booting up core 1 (0)
 running
cpu1: MPIDR=80000001
cpu1: MIDR=410fd034 Cortex-A53 r0p4
cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu1: L1 Icache 32K linesz=64 set/way=256/2
cpu1: L1 Dcache 32K linesz=64 set/way=128/4
cpu1: L2 Unified 1024K linesz=64 set/way=1024/16
board_smp_start: cpu_cluster_id: 0, cpu_id: 2
NOTTCE:  S32 T TA: s323pw_pdomrin_on: bootingnup cor  2u 0)
nning
cpu2: MPIDR=80000002
cpu2: MIDR=410fd034 Cortex-A53 r0p4
cpu2: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu2: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu2: L1 Icache 32K linesz=64 set/way=256/2
cpu2: L1 Dcache 32K linesz=64 set/way=128/4
cpu2: L2 Unified 1024K linesz=64 set/way=1024/16
board_smp_start: cpu_cluster_id: 0, cpu_id: 3
ngTICE:  SS32TT-A:: 32_pwr_rodain_on: booting up cpre 3 (0n
cpu3: MPIDR=80000003
cpu3: MIDR=410fd034 Cortex-A53 r0p4
cpu3: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu3: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu3: L1 Icache 32K linesz=64 set/way=256/2
cpu3: L1 Dcache 32K linesz=64 set/way=128/4
cpu3: L2 Unified 1024K linesz=64 set/way=1024/16
board_smp_start: cpu_cluster_id: 1, cpu_id: 0
NOTICE:  S32 TF-A: s32_pwr_domain_on: booting up core 4 (0)
NOTICE:  S32 TF-A: s32_pwr_domain_on_finish: cpu 4 running
cpu4: MPIDR=80000100
cpu4: MIDR=410fd034 Cortex-A53 r0p4
cpu4: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu4: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu4: L1 Icache 32K linesz=64 set/way=256/2
cpu4: L1 Dcache 32K linesz=64 set/way=128/4
cpu4: L2 Unified 1024K linesz=64 set/way=1024/16
board_smp_start: cpu_cluster_id: 1, cpu_id: 1
NOTICE:  S32 TF-A: s32_pwr_domain_on: booting up core 5 (0)
cpu 5 running
cpu5: MPIDR=80000101
cpu5: MIDR=410fd034 Cortex-A53 r0p4
cpu5: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu5: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu5: L1 Icache 32K linesz=64 set/way=256/2
cpu5: L1 Dcache 32K linesz=64 set/way=128/4
cpu5: L2 Unified 1024K linesz=64 set/way=1024/16
board_smp_start: cpu_cluster_id: 1, cpu_id: 2
NOTICE:  S32 TF-A: s32_pwr_domain_on: booting up core 6 (0)
nning
cpu6: MPIDR=80000102
cpu6: MIDR=410fd034 Cortex-A53 r0p4
cpu6: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu6: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu6: L1 Icache 32K linesz=64 set/way=256/2
cpu6: L1 Dcache 32K linesz=64 set/way=128/4
cpu6: L2 Unified 1024K linesz=64 set/way=1024/16
board_smp_start: cpu_cluster_id: 1, cpu_id: 3
NOTICE:  S32 TF-A: s32_pwr_domain_on: booting up core 7 (0)
7 running
cpu7: MPIDR=80000103
cpu7: MIDR=410fd034 Cortex-A53 r0p4
cpu7: CWG=4 ERG=4 Dminline=4 Iminline=4 VIPT
cpu7: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu7: L1 Icache 32K linesz=64 set/way=256/2
cpu7: L1 Dcache 32K linesz=64 set/way=128/4
cpu7: L2 Unified 1024K linesz=64 set/way=1024/16
 
System page at phys:00000000a0010000 user:ffffff8040315000 kern:ffffff8040311000
Starting next program at vffffff8060097300
ClockCycles samples:
 0 62957977
 1 62957977
 2 62957978
 3 62957977
 4 62957977
 5 62957977
 6 62957977
 7 62957977
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!!
Starting watchdog...
Starting serial driver ...
Starting Networking driver (/dev/socket)...
Starting SPI driver (/dev/spi0,1,2,3,4,5)...
Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)...
Starting USDHC0 memory card driver...
Path=Starting CAN driver...
0 - imx
 target=0 lun=0     Direct-Access(0) - SDMMC: AAM20E Rev: 1.0
#
#
#
# slog2info -c
 
Process 4117 (slog2info) exited status=0.
ghccu# slog2info -w &
[1] 12309
                                          random.4                  low     0  -----UNSYNC-----
                                          random.4                 high     0  -----UNSYNC-----
Jan 01 00:00:00.022                      console.3                           0  -----ONLINE-----
                                         console.3                  out     0  -----UNSYNC-----
Jan 01 00:00:00.027                       random.4                           0  -----ONLINE-----
                                          random.4              default     0  -----UNSYNC-----
Jan 01 00:00:00.028                    random.4..0                           0  -----ONLINE-----
                                       random.4..0                 slog     0  -----UNSYNC-----
Jan 01 00:00:00.050             devc_serlinflexd.7                           0  -----ONLINE-----
                                devc_serlinflexd.7                 slog     0  -----UNSYNC-----
Jan 01 00:00:00.055                   spi_master.8                           0  -----ONLINE-----
                                      spi_master.8               normal     0  -----UNSYNC-----
Jan 01 00:00:00.059                   spi_master.9                           0  -----ONLINE-----
                                      spi_master.9               normal     0  -----UNSYNC-----
Jan 01 00:00:00.063                  spi_master.10                           0  -----ONLINE-----
                                     spi_master.10               normal     0  -----UNSYNC-----
Jan 01 00:00:00.067                  spi_master.11                           0  -----ONLINE-----
                                     spi_master.11               normal     0  -----UNSYNC-----
Jan 01 00:00:00.088             devb_sdmmc_mx8x.17                           0  -----ONLINE-----
                                devb_sdmmc_mx8x.17                 slog     0  -----UNSYNC-----
Jan 01 00:00:04.268                       qconn.20                           0  -----ONLINE-----
                                          qconn.20                 slog     0  -----UNSYNC-----
#
#
#
# io-pkt-v6-hc -p tcpip pkt_typed_mem=pfe_ddr -d /proc/boot/devnp-pfe-2.so class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw
# Jan 01 00:00:14.060                    iopkt.16408                           0  -----ONLINE-----
Jan 01 00:00:14.060                    iopkt.16408          main_buffer*     0  detect_armv8ce_hw: armv8ce is supported!
Jan 01 00:00:14.061                    iopkt.16408          main_buffer      0  tcpip starting
Jan 01 00:00:14.062                    iopkt.16408          main_buffer      0  smmu support is disabled
Jan 01 00:00:14.063                    iopkt.16408          main_buffer      0  initializing IPsec...
Jan 01 00:00:14.063                    iopkt.16408          main_buffer      0   done
 
Jan 01 00:00:14.064                    iopkt.16408          main_buffer      0  IPsec: Initialized Security Association Processing.
 
Jan 01 00:00:14.067                    iopkt.16408          main_buffer      0  /proc/boot/devnp-pfe-2.so class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw
Jan 01 00:00:14.068             io_pkt_v6_hc.16408                           0  -----ONLINE-----
Jan 01 00:00:14.068             io_pkt_v6_hc.16408                 slog*     0  INF[src/pfe_drv.c:1346]: VERSION INFO
        Driver version: 1.8.0
        Driver commit hash: 57b6eefdb35cbff7a43ecfbdca3334760b1d0553
        PFE_CFG_MULTI_INSTANCE_SUPPORT: 0
        PFE_CFG_LOCAL_IF: 6
        PFE_CFG_MASTER_IF: 6
        PFE_CFG_SC_HIF: 1
        PFE_CFG_HIF_RING_LENGTH: 256
        PFE_CFG_PFE0_PROMISC: 1
        PFE_CFG_PFE1_PROMISC: 1
        PFE_CFG_PFE2_PROMISC: 1
 
 
Jan 01 00:00:14.068             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_drv.c:1353]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed.
 
Jan 01 00:00:14.068             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_fw.c:94]: 45724 bytes read
 
Jan 01 00:00:14.068             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_fw.c:100]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw
 
Jan 01 00:00:14.068             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_fw.c:94]: 23352 bytes read
 
Jan 01 00:00:14.069             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_fw.c:100]: Loaded firmware file: /proc/boot/s32g_pfe_util.fw
 
Jan 01 00:00:14.069             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_drv.c:1449]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII.
 
Jan 01 00:00:14.069             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_drv.c:1449]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII.
 
Jan 01 00:00:14.069             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_drv.c:1449]: MII mode configuration for pfe2/EMAC2 not found. Using SGMII.
 
Jan 01 00:00:14.069             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_drv.c:1467]: Issuing PFE peripheral reset...
 
Jan 01 00:00:14.179             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_drv.c:1468]: PFE reset OK.
 
Jan 01 00:00:14.179             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2826]: PFE CBUS p0x46000000 mapped @ v0x1e2a574000 (0x1000000 bytes)
 
Jan 01 00:00:14.179             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2831]: HW version 0x101
 
Jan 01 00:00:14.179             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_hw_feature.c:95]: Silicon S32G3
 
Jan 01 00:00:14.179             io_pkt_v6_hc.16408                 slog      0  WRN[hw/s32g/pfe_platform_master.c:2843]: Fail-Stop mode disabled
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2093]: PFE_ERRORS:Parity instance created
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2108]: PFE_ERRORS:Watchdog instance created
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2124]: PFE_ERRORS:Bus Error instance created
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2137]: PFE_ERRORS:FW Fail Stop instance created
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2150]: PFE_ERRORS:Host Fail Stop instance created
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2163]: PFE_ERRORS:Fail Stop instance created
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:2176]: PFE_ERRORS:ECC Err instance created
 
Jan 01 00:00:14.254             io_pkt_v6_hc.16408                 slog      0  INF[hw/s32g/pfe_platform_master.c:1097]: BMU1 buffer base: p0xc0000000
 
Jan 01 00:00:14.255             io_pkt_v6_hc.16408                 slog      0  ERR[src/oal_mm_qnx.c:98]: (DRIVER) event 1 - Driver runtime error: mmap64() failed: 1
 
Jan 01 00:00:14.255             io_pkt_v6_hc.16408                 slog      0  ERR[src/oal_mm_qnx.c:171]: (DRIVER) event 1 - Driver runtime error: Can't get memory block
 
Jan 01 00:00:14.255             io_pkt_v6_hc.16408                 slog      0  ERR[hw/s32g/pfe_platform_master.c:1125]: (DRIVER) event 1 - Driver runtime error: Unable to get BMU2 pool memory
 
Jan 01 00:00:14.256             io_pkt_v6_hc.16408                 slog      0  ERR[src/pfe_drv.c:1529]: (DRIVER) event 1 - Driver runtime error: Unable to initialize the platform
 
Jan 01 00:00:14.257                    iopkt.16408          main_buffer      0  Unable to init /proc/boot/devnp-pfe-2.so: No such device
 
Jan 01 00:00:14.257             io_pkt_v6_hc.16408                 slog      0  INF[src/pfe_drv.c:1302]: PFE entry failed, PFE driver terminated
 
 
#
#
#
#
#
#
 
 
Re: PFE on S32G A53 QNX ERROR

Hello, @SandalWood 

I feel very sorry for late response.

Not sure if the issue has been resolved?

May I know if there was a environment variable skip_scmi_reset_agent set in your uboot?

If not, try setting the following: "setenv skip_scmi_reset_agent '1'"


BR

Chenyin

 


Re: PFE on S32G A53 QNX ERROR

Hello, @SandalWood 

Thanks for the reply.

1. I suggest reviewing the "PFE_QNX_DRV_IntegrationManual.pdf", which is included in PFE driver release package and assure that each step(Building, Running driver) is correct.

2. If the DTB file worked well in Linux, then the original one in QNX should be replaced with it.

Would you mind trying it again and let me know the test result.


BR

Chenyin

Re: PFE on S32G A53 QNX ERROR

Hello, @SandalWood 

Thanks for you reply.

Yes, I understand the situation now.

Will investigate it and reply you later when there are any findings.


BR

Chenyin

Re: PFE on S32G A53 QNX ERROR

1.The location of the pfe DDR cannot use the example provided in the NXP manual and must be changed to an idle location to prevent overlap with the reserved memory.

2.I haven't made any dynamic changes.My run cmd is:io-pkt-v6-hc -p tcpip pkt_typed_mem=pfe_ddr -d /proc/boot/devnp-pfe-2.so pfe0_link=1000-1-3,pfe0_mac=025556000050,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw

And I did not make any dynamic changes, I did not modify the environment variables of uboot. Linux and QNX use the same uboot image. So, I understand that the configuration of Serdes on QNX should be the same as Linux, right? 

Re: PFE on S32G A53 QNX ERROR

Hello, @SandalWood 

Glad that the ddr issue resolved, would you mind sharing the reasons?

For the ping issue mentioned, have you mentioned the driver limitation below:

chenyin_h_0-1757056879842.pngchenyin_h_0-1757056879842.png


BR

Chenyin

Re: PFE on S32G A53 QNX ERROR

Hi,
We have resolved the ddr error, but there may be an new issue during ping.
The pfe0 in our board is directly connected to the external swtich through MAC-TO-MAC(SGMII MODE). In a Linux environment, this link is normal and can communicate with the external environment normally, such as ping being OK. But after replacing Linux with the current QNX, the ping problem will occur.
In Linux, we changed the device tree and configured pfe0 to fix sgmii mode. I suspect it's related to this, but I don't know how to configure it in QNX。
The log please see the attach.


Re: PFE on S32G A53 QNX ERROR

160 is hex 0xa0,it seems that pfe_ddr is ok

# pidin sys=asinfo
Header size=0x00000108, Total Size=0x00001050, #Cpu=8, Type=257
Section:asinfo offset:0x00000b90 size:0x00000200 elsize:0x00000020
0000) 0000000000000000-0000ffffffffffff o:ffff a:0010 p:100 c:0 n:/memory
0020) 0000000000000000-00000000ffffffff o:0000 a:0010 p:100 c:0 n:/memory/below4G
0040) 0000000080000000-00000000ffffffff o:0020 a:0017 p:100 c:0 n:/memory/below4G/ram
0060) 0000000880000000-00000008dfffffff o:0000 a:0017 p:100 c:0 n:/memory/ram
0080) 00000000ff800000-00000000ff83afff o:0040 a:0005 p:100 c:0 n:/memory/below4G/ram/atf
00a0) 0000000080000000-0000000083ffffff o:0040 a:0007 p:100 c:0 n:/memory/below4G/ram/pfe_ddr
00c0) 0000000050800000-000000005080ffff o:0000 a:0003 p:100 c:0 n:/memory/gicd
00e0) 0000000050900000-00000000509fffff o:0000 a:0003 p:100 c:0 n:/memory/gicr
0100) 0000000088000080-0000000088007fff o:0040 a:0005 p:100 c:0 n:/memory/below4G/ram/fdt
0120) 00000000800d10a8-00000000815fa8b3 o:0000 a:0005 p:100 c:0 n:/memory/imagefs
0140) 0000000080080fa0-00000000800d10a7 o:0000 a:0007 p:100 c:0 n:/memory/startup
0160) 00000000800d10a8-00000000815fa8b3 o:0000 a:0007 p:100 c:0 n:/memory/bootram
0180) 00000000a0000000-00000000a0007fff o:0040 a:0007 p:100 c:0 n:/memory/below4G/ram/sysram
01a0) 00000000a0014000-00000000ff7fffff o:0040 a:0007 p:100 c:0 n:/memory/below4G/ram/sysram
01c0) 00000000ff83b000-00000000ffffffff o:0040 a:0007 p:100 c:0 n:/memory/below4G/ram/sysram
01e0) 0000000880000000-00000008dd5e2fff o:0060 a:0007 p:100 c:0 n:/memory/ram/sysram

Re: PFE on S32G A53 QNX ERROR

Hello, @Chen 

Thanks for reply.The return code see the log.

SandalWood_0-1757049933250.pngSandalWood_0-1757049933250.png

SandalWood_1-1757049947809.pngSandalWood_1-1757049947809.png



BR

SandalWood 

Re: PFE on S32G A53 QNX ERROR

Hello, @SandalWood 

Thanks for the post.

Seems the memory is not correctly mapped, may I know if there is a log indicating that as_add_containing() was successful called?


BR

Chenyin

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:05 AM
更新者: