2162125_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2162125_en-US

2162125_en-US

NVM Service Status "Dead" After Migration to NXP Linux Package 25.Q2 6.6

Dear NXP,

After migrating to the NXP Linux Package 25.Q2 6.6 , we have observed that the NVM service status is "dead" following startup attempts as below screenshot

fawaz_0-1756812390910.png

Could you please advise on possible causes for the NVM service failing to run, and provide any troubleshooting steps or documentation relevant to this issue in the NXP Linux Package 25.Q2 6.6?

Thank you for your assistance.

SecurityRe: NVM Service Status "Dead" After Migration to NXP Linux Package 25.Q2 6.6

Hi @fawaz!

Thanks for the update!

It looks like you already have an active thread in a private community. Since the i.MX95 is not yet available to all customers, support for it is being handled through a specialized channel.

Your case will continue through the original post to ensure consistency and proper follow up. If you haven’t received a response there, I’ll escalate it to help move things forward.

Best regards,
Chavira

Re: NVM Service Status "Dead" After Migration to NXP Linux Package 25.Q2 6.6

Dear  @Chavira 

We are using BSP version 6.6.52 on the chm-imx95-evk board, with an imx95 (aarch64) processor. The Linux version is 6.6.52-lts-next-g57d80ee0fb86-dirty. 

Rev.A CHM board

fawaz_0-1756876633904.png

To reproduce the issue:

1) Boot the board with the mentioned BSP and Linux version.
2) Attempt to start the NVM service.
3) Observe that the NVM service status is "dead"

fawaz_1-1756876718201.png


Thank You..!



Re: NVM Service Status "Dead" After Migration to NXP Linux Package 25.Q2 6.6

Hi @fawaz,

Thank you for reaching out to NXP Support!

To assist you more effectively, could you please confirm the following details:


Are you using BSP version 6.6.36 or 6.6.52?

What processor are you working with?

What is the board you are using?

Could you describe the steps you are following to reproduce the issue on your side? This will help me replicate it accurately.


Best regards,
Chavira

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-20-2025 01:46 PM
更新者: