Hello ,
I'm trying to test I2C master on S32K324 but i'ts not working.
Actually I have no I2C slave connected to I2C master but I don't see any transition on PTD13 (LPI2C_SDA) or PTD14 (LPI2C_SCL), the two pins are ever HIGH.
I expect to see start condition like attached file.
Attached there is the project.
Regards, Francesco.
Hi @francescovico,
It does work on my side - I have tested your code.
If it does not work on you side, explain in details what does not work.
Make sure the DBGEN bit is set at the time the transfer is called.
Have you tested it with CM7_1 running?
Do you use external pull-up resistors?
Regards,
Daniel
Hi Daniel,
It still not working well .
Regards, Francesco.
HI @francescovico,
danielmartynek_0-1756971786422.png
Enable it after the Init function.
Otherwise, the Init function will clear the bit.
Regards,
Daniel
Hello Daniel,
sorry but putting:
IP_LPI2C_0->MCR |= LPI2C_MCR_DBGEN_MASK;
The I2C still not working.
Attached my project.
Regards, Francesco.
Hi @francescovico,
When CM7_1 is halted, the MCU enters debug mode.
To ensure LPI2C continues functioning, either set the DBGEN bit in LPI2C_MCR to allow operation during debugging, or Keep CM7_1 running.
BR, Daniel
Hello Daniel,
Thank you, it's true I forgot to initialize interrupt.
Also with interrupt enabled the I2C it's not working.
Attached there is the project with interrupt enabled.
Do you have other suggestions?
Regards.
Hello Francesco,
I haven't tested the code, but I see that you did not enable the LPI2C interrupt.
Add IntCtrl_Ip driver with LPI2C0_Master_Slave_IRQHandler.
And initialize the driver in the code.
Regards,
Daniel