2159336_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2159336_en-US

2159336_en-US

FS32K116LAT0MLFT/FS32K116LAT0MLFR top marking and package specification

Hello,

Could you please help me to validate the meaning  of top marking?

Row 1-2: FS32K116LAM-> last M whats mean?

Row 3: ON96V

Row 4: CTVREB 

Also please help me with quadrant position for tray or tape package.


Re: FS32K116LAT0MLFT/FS32K116LAT0MLFR top marking and package specification

Hi @cynthia_pinto,

The letter M shows the temperature range (-40 °C to 125 °C). You can refer to the S32K data sheet's chapter 3.2 (ordering information):

Snag_559ab02.png

You can also refer to the spreadsheet attached to the data sheet (S32K1xx_Orderable_Part_Number_List.xlsx) for a list of standard orderable parts:

Snag_55aacc2.png

The row 3 & 4 markings refer to internal coding.

Finally, packaging information should be displayed in the "Buy Options" page: FS32K116LAT0MLFT Product Information | NXP Semiconductors.

Best regards,
Julián

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 06:02 PM
更新者: