Hi,
I am working with the S32G274ARDB2 image, where I have enabled Xen hypervisor support as per the guidelines in the Linux BSP 38.0 User Manual. After building the image, I observed the following output from the `lsblk` command in the Xen environment:
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mmcblk0 179:0 0 14.8G 0 disk
|-mmcblk0p1 179:1 0 64M 0 part
|-mmcblk0p2 179:2 0 980M 0 part /
|-mmcblk0p3 179:3 0 980M 0 part
`-mmcblk0p4 179:4 0 980M 0 part
Hello @hulk101,
Were you able achieve your goal with the information I provided?
If so, please select my last reply as an accepted solution, if not, please let me know if you encounter any errors.
Thanks!
Hello @hulk101,
Xen is not an NXP product and therefore I cannot offer you much support about it. However, here is some information that you might find useful. Dom0 has default access to all hardware resources, this includes SD/eMMC partitions (mmcblk0p1, mmcblk0p2, mmcblk0p3, ...), although it might be possible to restrict access to Dom0 I would not recommend it since Dom0 is intended to create all other domains (like Domu). DomU does not have access to all hardware resources by default, for example for partitions, you can dynamically attach them by running:
xl block-attach domu1 phy:/dev/mmcblk0p3 xvdb w
or to detach them:
xl block-detach domu1 xvdb
You can also add those commands in the configuration files of the configuration file of domu1.
Please note that the commands might change slightly depending on the partitions needed and the domain names.
This way the partition will appear in domu1 in:
/dev/xvdb
There are some configuration you can perform in the device tree, however for the requirements you have it does not seem that it would be the correct approach, however, please check https://wiki.xenproject.org/wiki/Device_tree.
Let me know if you have more questions.