2152392_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2152392_en-US

2152392_en-US

S32K5 RTD configuration does not allow to set initial value in some pins

Hello,


Some pins as the ones listed below don't allow to set the initial value when being configured. Is there a reason for that?

nxp52415_0-1755178285308.png


nxp52415_1-1755178333678.png


Regards

RTDRe: S32K5 RTD configuration does not allow to set initial value in some pins

Hi @nxp52415,

As I said, with pins that you selected, they are not supported this function. So, the "the initial value" is not necessary for these pins. Default, RTD driver disabled "the initial value" on "pins were not supported RCVR", and these pins will be generated "the initial value" as 0. Even when driver allow user configures RCVR for these pins, then it doesn't have any effection because it has not support RCVR.

Best regards,

Dan

Re: S32K5 RTD configuration does not allow to set initial value in some pins

Hi Dan,

I was talking about the initial value and not the RCVR. Can you explain why the initial value cannot be set in these pins?

Regards 

Re: S32K5 RTD configuration does not allow to set initial value in some pins

Hi @nxp52415,

This is the information about "Receiver Select" bit in S32K5 RM:

DanNguyenDuy_0-1755499600839.png

You can find the pins support the RCVR in the "IO Signal Table" sheet in the S32K56x_IOMUX.xlsx (attached file in S32K5RM).

And based on this files, pins that you showed as not support RCVR.

DanNguyenDuy_1-1755499842288.png

Best regards,

Dan

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 12:49 AM
更新者: