2152291_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2152291_en-US

2152291_en-US

FRDM-MCXA156 – mcuboot_opensource SDK Example Not Working in MCUXpresso

Hi,

I am currently working with the FRDM-MCXA156 board for evaluation of one of

our projects and using the SDK examples in MCUXpresso IDE.
I have tested basic examples such as:


  • frdmmcxa156_blink_led

  • frdmmcxa156_lpuart_interrupt_transfer

 These examples worked as expected.


However, while testing the frdmmcxa156_mcuboot_opensource example from the

same SDK, I encountered the following log message on the terminal:



Screenshot 2025-08-14 145505.pngScreenshot 2025-08-14 145505.png


I have followed the tutorial from the official documentation here:

link


Could you please suggest what might be causing this issue?






Core and MemoryFRDM-TrainingRe: FRDM-MCXA156 – mcuboot_opensource SDK Example Not Working in MCUXpresso

Hi @CEPL_Dev ,

you can also use Secure Provisioning Tool, see step-by-step procedure described in the user guide: Generic workflows — MCUXpresso Secure Provisioning Tool 25.06

Re: FRDM-MCXA156 – mcuboot_opensource SDK Example Not Working in MCUXpresso

Hello @CEPL_Dev 

Thanks for your question.

Please use the two projects together: "mcuboot_opensource" and "ota_mcubot_basic".
 
For detailed steps, please refer to readme.md.

Alice_Yang_0-1755166872242.pngAlice_Yang_0-1755166872242.png

If still have issue, please show all your steps, I help you check.

Thank you.


BR

Alice


Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 02:52 PM
Updated by: