2151587_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2151587_en-US

2151587_en-US

issue in flashing bin file from U-MULTILINK-FX

Hello NXP team,

I am using KW45 bare MCU and with help of  U-MULTILINK-FX trying to flash .bin file but ,after successful flash through MCUXpresso IDE V24.12.148 using SWD warning message come in console. Can NXP tell me reason for the issue?

I would like to highlight I am successfully able to flash any axf file generated after project build successfully using same U-MULTILINK-FX and MCUXpresso IDE V24.12.148 through SWD.


I am sharing you part of console warning below.

Mode is In-Circuit Debug.
(C)opyright 2012, P&E Microcomputer Systems, Inc. (www.pemicro.com)
API version is 101
TARGET XML PATH is C:\nxp\MCUXpressoIDE_24.12.148\ide\plugins\com.pemicro.debug.gdbjtag.pne_5.9.5.202412131551\supportFiles_ARM\target_v8m_vfp_se.xml
Server 1 running on 127.0.0.1:7224
Server 2 running on 127.0.0.1:7226
Server 3 running on 127.0.0.1:7228
Server 4 running on 127.0.0.1:7230
Server 5 running on 127.0.0.1:7232
Server 6 running on 127.0.0.1:7234
Server 7 running on 127.0.0.1:7236
Server 8 running on 127.0.0.1:7238
Server 9 running on 127.0.0.1:7240
Server 10 running on 127.0.0.1:7242
Warning: No data was programmed in FLASH

with regards

Chetan

Re: issue in flashing bin file from U-MULTILINK-FX

Hello,

Hope you are doing well.


Could you give me more information about your application? What SDK Version are you using and are you using an SDK example? If so, did you implement any modifications?

Could you provide us with more information about the procedure you are following in order to get this warning?


When you mention that you are able to flash using .axf files, how are you testing this? Were you able to run an SDK example afterwards?


This warning might be due to an incompatibility with the external debugger.


Best Regards,

Ana Sofia.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 12:52 AM
Updated by: