2151032_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2151032_en-US

2151032_en-US

iMX8MP eqos not working for 10base-t

Hello,

Since we introduced the Verdin iMX8MP SoM, we knew that the 10base-t speed wasn't working on the ethernet port that's included in the SoM. This ethernet port is connected to the eqos MAC and we include a KSZ9131 PHY. At first, we thought this would be a software bug, but even the latest upstream kernel (currently .17-rc1) still presents the same issue.

On a web search I found this thread: https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ethernet-eqos-ksz9131-can-link-but-ping-fail-at...


In the solution, they mention that the reason for the failure is the fact that the KSZ9131 removes the preamble bytes, which it does. However, the Errata ERR050694 states (emphasis mine):

"However due to the defect, in configurations where frame preemption is enabled, when preamble byte does not precede the SFD, SMD-S, or SMD-C byte, the received packet is discarded by the MAC receiver"

I checked, and could only find that frame preemption is enabled when using the traffic shaping utilities, so no frame preemption enabled by default. 

Could someone confirm that the Errata ERR050694 applies even when frame preemption is disabled? 

Re: iMX8MP eqos not working for 10base-t

Thank you for your response!

I verified that after setting bit 2 in register 0x11, data started flowing in 10BaseT mode.

Re: iMX8MP eqos not working for 10base-t

Hi,

Thank you for your interest in NXP Semiconductor products,

According to the IP experts, when the PHY removes the preamble, EQOS discards the packet. The PHY must be configured to send the preamble.

It was revealed by Microchip that there is a reserved bit (register 0x11, bit 2 is marked read-only in the datasheet) that prevents the preamble removal in 10Mbps mode, allowing this to work.

Regards

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 06:10 PM
更新者: