HI
I'm trying to connect pn7161 with esp.
but I'm failed
my question is any initial firmware i must burn in begging or dirictly i can connect IC with any another board
Hello @user_ahmed
You can get the latest FW from nfc-NXPNFCC_FW/InfraFW/pn7160/12_50_11 at master · NXP/nfc-NXPNFCC_FW · GitHub
PN7161 does not have working firmware in RAM. it tries to upload firmware, but in my setup the firmware file is missing. so i need your help find/download the correct firmware array from NXP’s package where the basic file in package that i need thanks
Hello @user_ahmed
It's recommended that you can refer to SW6705 - PN7160 NXP-NCI MCUXpresso Example Project, which is based on MCU projects.
Please log in Plug-n-Play NFC Frontend with Integrated Firmware | NXP Semiconductors to download it.
Hello @user_ahmed
PN7160/1 is a frond-end product, which cannot work alone, must work together with Host, like MCU. So, you mentioned "esp", is it a type of Host? if so, esp can communicate with PN7161 via I2C or SPI.
Also, you bought the IC, which has default FW, when it worked with the Host, its FW can be updated to the latest version.