2149920_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2149920_en-US

2149920_en-US

MIMXRT1160 Unique ID eFuse

MIMXRT1160 has a 64-bit Unique ID fuse at 0x900-0x910. Can the value be used as device unique ID, or is it "unique" across processor/batches? If that's the case, is there another pre-programmed register or fuse which can be used as device unique ID?

Thanks

Re: MIMXRT1160 Unique ID eFuse

Hi @tbonkers ,

Thanks for your updated information.

Regarding "My requirement is to have an unique ID for each device, and I was thinking that it would be great if I can use the value of the fuse 0x900."

Are you saying that you used the value of fuse 0x900, a 32-bit data? If so, I don't think that's a good choice, 32-bit data is not unique . 

But if you use the fuse values 0x900 and 0x910, the 64-bit data is unique (unique ID), which would be Okay.

Wish it helps you.

Best Regards
MayLiu

Re: MIMXRT1160 Unique ID eFuseHi,
My requirement is to have an unique ID for each device, and I was thinking that it would be great if I can use the value of the fuse 0x900.
From your response I understand that the value of the fuse is indeed unique for each unit - please correct me if I'm wrong.
Thanks
Re: MIMXRT1160 Unique ID eFuse

Hi @tbonkers ,

Thank you so much for your interest in our products and for using our community.

 Yes, IMXRT1160 has a 64-bit Unique ID which configuration  by NXP.

mayliu1_0-1754970106981.pngmayliu1_0-1754970106981.png

Regarding "If that's the case, is there another pre-programmed register or fuse which can be used as device unique ID?"

Could you tell me more details of your requirement?  In IMXRT1160 already provide a 64 bit  device unique ID fuse at 0x900-0x910.

mayliu1_1-1754970965556.pngmayliu1_1-1754970965556.png

Best Regards

MayLiu

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 11:42 PM
更新者: