2149812_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2149812_en-US

2149812_en-US

I am starting with LPC Expresso IDE software for coding LPC2478 controller

I had done all things free addition is start But when I code run this problem is occurs this are the errors so please guide me 16:19:29 **** Incremental Build of configuration Debug for project LED_Blink **** make -r all bash.exe: warning: could not find /tmp, please create! Building file: ../src/main.c bash.exe: warning: could not find /tmp, please create! Invoking: MCU C Compiler arm-none-eabi-gcc -DDEBUG -D__CODE_RED -D__REDLIB__ -O0 -fno-common -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=arm7tdmi -specs=redlib.specs -MMD -MP -MF"src/main.d" -MT"src/main.o" -MT"src/main.d" -o "src/main.o" "../src/main.c" bash.exe: warning: could not find /tmp, please create! ../src/main.c:1:64: fatal error: LPC24xx.h: No such file or directory compilation terminated. make: *** [src/main.o] Error 1 16:19:30 Build Finished (took 300ms)

LPCXpresso ForumRe: I am starting with LPC Expresso IDE software for coding LPC2478 controller

Hi@VijayaJangam1 

The FT232RL is a USB-to-UART bridge chip.

It only provides a serial port connection for communication.

It cannot provide hardware debug, because it does not support ARM debug protocols.

If it’s debugging, I’ll suggest connecting an LPC-Link2.

BR

Harry

Re: I am starting with LPC Expresso IDE software for coding LPC2478 controller
Hello Sir,
  I had include LPC24xx.h file in the project and starting with LED program but  I had faced problem in Debugging there is not properly Debug the project What I should do next please guide me. I have sending the document in that mention all things 
Thank You for your Support 
 
 
 
 
Re: I am starting with LPC Expresso IDE software for coding LPC2478 controllerThank You for your Support
Re: I am starting with LPC Expresso IDE software for coding LPC2478 controller

Hi @VijayaJangam1 

1.The "bash.exe: warning: could not find /tmp" means your Windows environment  doesn’t have a /tmp directory.

I think you can try to create a tmp folder.

2.fatal error: LPC24xx.h: No such file or directory

means your project can’t find the LPC2478 MCU header file.

I think you can try to add the include path to your project settings or 

copy the file into your project’s include directory.

BR

Harry

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 12:59 AM
更新者: