Hello,
I’m trying to use the s32z2e2_flash_MX25UW25A45G.py Python script provided by the MBDT team to flash to the S32E2 via QSPI. This script can be used with the gdb command line or with S32 Design Studio/ S32 Debug Probe. Are there any resources or documentation on the S32 Debug probe, or setting up GDB with the debug probe or within S32DS, that would be helpful for running and debugging this flashing script?
Thanks!
Tasnia
Hi,
I'm not familiar with MBDT, but S32DS contains it's own script for MX25UW25A45G. You can select it from S32DS Debug Configurations
In attachment is script itself, you can compare it with yours one.