2148060_zh-CN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2148060_zh-CN

2148060_zh-CN

32DS3.4安装问题

安装过程中装S32K3xx development package是遇到问题,见图片有道截屏翻译结果_1754544132351.png

Re: 32DS3.4安装问题我这边安装SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite实时驱动 现在编译没有问题了Re: 32DS3.4安装问题

请问是已经安装完S32K3 RTD 3.0.0了? 有没有根据工程里那个description.txt描述的Update Code?

Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...). Clicking on any one of those will generate all the components. Make the desired changes(if any) then click on the menu "ConfigTools->Update Code".

Re: 32DS3.4安装问题

你好 我就在你给我的这里有一些FAE做的RTD3.0.0的示例 All Example S32K312 DS3.5 RTD-3.0.0下载了个S32K312_UART_DMA的程序后  辨析报错了如下图630a34eb-a0b7-4052-9206-4705ae29e287.png



Re: 32DS3.4安装问题

从S32K3 RTD 2.0.3之后,RTD就没有再包含S32K312的demo了。  网上能找到一些S32K312的示例,但都不像S32K344那样包含各个外设模块。

这里有一些FAE做的RTD3.0.0的示例 All Example S32K312 DS3.5 RTD-3.0.0

请问你按照我之前给你的链接,还能下载到RTD2.0.x吗?“Previous” tab里也找一下。

Re: 32DS3.4安装问题你好 我这边S32DS3.6.3安装好了 我这边买的S32K312MINI-EVB开发板 请问官网的demo程序在哪块找?Re: 32DS3.4安装问题好的 我装一个新的版本试试Re: 32DS3.4安装问题

Hi

抱歉 我看你之前是想要在S32DS v3.6.1里安装S32K3 RTD 2.0.x。 但如果你以前没下载过旧版本RTD的话,可能现在只能看到几个更新版本的RTD了。

点击 S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M

S32DS v3.6.x开始安装RTD简化了很多,只需要照着Offline Package Installation Setup步骤选择下载好的RTD离线包(_DesignStudio_updatesite.zip)就行了。

不建议使用S32DSv3.4这么旧的版本,现在的S32DS已经升级到v3.6.3了。


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 07:49 AM
更新者: