2148026_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2148026_en-US

2148026_en-US

IW610 RF_CNTL Pins for FEM Control

Hi there,

I am looking to use the IW610 with an external front-end module (FEM). As per the datasheet (see attached image), the IW610 has RF_CTRL pins to be used with components such as FEMs

However, the exact function of these pins (I am assuming one will go high on RF Tx, and one will go high on RF Rx) is not stated. Where can I find the information on this please?

Or is this something that is customisable and set up in the drivers?

Thanks,

Iain.

Re: IW610 RF_CNTL Pins for FEM Control

Hello @iain_hpsnz 


The document is confidential, you could submit a ticket to nxp to sign NDA with us. Then you can get access.


Best Regards

Shaun

Re: IW610 RF_CNTL Pins for FEM Control

Hey Shaun,

Thanks for coming back to me so quickly. The design guide sounds interesting and is something I would like to take a look at, however when I click your link I am given the error:

Your userId does not have sufficient privilege to proceed with download.

Any idea why this would be?

Our case is small, perhaps 100 units per year, so I am assuming you deem this to be not worth your time.

Assuming that this is the case, does that mean that this FEM control feature is completely unavailable to me? There is no way to set this up through the existing driver using, or using an existing example?

I notice the IC has an onboard PA/LNA to act as an internal FEM - can this be controlled via the driver?

Thanks,

Iain.

Re: IW610 RF_CNTL Pins for FEM Control

Hello @iain_hpsnz 


We provide some reference design in Design guide, if you want similar configuration, you may follow the guide to design: https://www.nxp.com/webapp/Download?colCode=AN14419&appType=license.

For custom design, we didn't release guide about FEM CTRL pin. You need to send your project info and design to nxp. We will evaluate your case and design. Then custom a FEM control calibration file to you. But it wastes time and request volume of project. Not recommended.


Best Regards

Shaun

Re: IW610 RF_CNTL Pins for FEM Control

Hi NXP

I am in need of the same information.

It seems very strange that you sell an evaluation board with the capability of using an external antenna, but how to switch to use it is confidential information.

Where/how do i sign such a NDA?

Regards
Tonny 


Tags (1)
No ratings
Version history
Last update:
‎08-15-2026 02:27 AM
Updated by: