2145231_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2145231_en-US

2145231_en-US

MCXA153 ADC TRIGGER

Dear all,

I'm developing a project based on the MCXA153VLH microprocessor.

It needs to sample an incoming analog voltage at regular intervals. I thought of using a timer to trigger the ADC to start the conversion.

I know that the ADC module of the MCXA153VLH microprocessor supports up to 4 hardware triggers, but I can't figure out the correspondence between the hardware peripheral and its specific trigger.

By analyzing the demo software provided with the SDK, I understand that Trigger 1 is associated with an IRQ generated by a pin. Which trigger is associated with a timer?

Thank you for your help and cooperation
regards


Re: MCXA153 ADC TRIGGER

Hello @_Ferrari_ 


Sorry for replying to you late on this thread.

Fortunately, I have already answered this for you in your other thread.

If anyone else has the same issue, please refer to:

https://community.nxp.com/t5/MCX-Microcontrollers/MCXA153VLH-ADC-trigger/td-p/2155041 


BR

Alice


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 06:16 PM
Updated by: