2144930_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2144930_en-US

2144930_en-US

Questions about the IW612 test content(UM11717)

Question about UM11717
1.Is PRBS the same as PRBS9, which means pseudorandom binary sequence of order 9?
  (UM11717 P.87, 89)

2.Please tell me the specifics of Whitening (UM11717 P.87-90 )

3.There is an error in the example for the receive antenna number setting command. Is this a mistake? (UM11717 P.51-59, 61, 64-66)
Example
10 0 2 2 // Set both TX and RX to antenna 2 (p. 27) → 10 2 2

4.If I input the Tx/Rx command sequences for 802.11b, g, a, n, ac, and ax in order, will I get the correct count?
Also, I don't know when the counting starts, so please let me know. (UM11717 P.51-60)


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 01:17 AM
Updated by: