2144678_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2144678_en-US

2144678_en-US

MIMXRT1176DVMAA - Not detecting over the JTAG

Hi Team

We developed a custom board based on MIMXRT1176DVMAA, and unfortunately,  device could not detecting over the JTAG.

During my troubleshooting, I found that internal LDO output "VDDA_1P0" (Pin N11) is not showing voltage (0V) and this output connected to VDD_MIPI_1P0 (Pin F10) DSI lines interface.

Could this be a problem preventing the device detecting over JTAG?

Verified the PMIC power sequence, all voltage rails sequence is as per the datasheet recommended.

Thanks.

Regards,

Gopala

Re: MIMXRT1176DVMAA - Not detecting over the JTAG

Hi @gopalakrishna ,

Thank you so much for your interest in our products and for using our community.

Regarding "During my troubleshooting, I found that internal LDO output "VDDA_1P0" (Pin N11) is not showing voltage (0V) and this output connected to VDD_MIPI_1P0 (Pin F10) DSI lines interface."

Could you provide more detailed information? Have you followed the design of the MIMXRT1170-EVKB board?

mayliu1_0-1754273865087.png

mayliu1_1-1754273906218.png

https://www.nxp.com/webapp/Download?colCode=MIMXRT1170HDUG

Please refer to the user guider "Hardware Development Guide for the MIMXRT1160/1170 Processor"

particularly Chapter 3 "Power Supply," to confirm whether your board design complies with the requirements outlined in Table 1 "Processor Power Supply Capacitors When Using On-Chip DC-DC Regulators."

Did you add 1 ms R/C delay , DCDC_PSWITCH should delay 1 ms with respect to DCDC_IN to guarantee that DCDC_IN is stable before the DC-DC starts up.

mayliu1_2-1754274637007.png

Please use an oscilloscope to measure the power-up sequence of the RT1170.

mayliu1_3-1754274756152.png


Best Regards

MayLiu

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:02 AM
Updated by: