2144170_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2144170_en-US

2144170_en-US

TJA1043 application

Hi, I have a question about the application schematic of TJA1043 (page 19):

The TJA1043's INH pin controls the enable pin of the 5V power supply chip that supplies power to the TJA1043's VCC pin, so when INH pulls down the enable pin of the 5V power supply chip, the 5V power supply chip can't supply power to the TJA1043's VCC pin, and there is no power supply to the TJA1043, so how can it output the INH signal to pull up the enable of the 5V power supply chip?

Re: TJA1043 applicationthank youRe: TJA1043 application

right


Re: TJA1043 application

您给的资料中提到了While the microcontroller is completely un-powered (no VCC supply),
the TJA1043 keeps partly alive via its battery supply. It allows the transceiver to monitor
the bus for CAN messages。我理解这就是TJA1043可以在没有VCC的情况下继续监听总线报文的原因吧

Re: TJA1043 application

Sleep mode VCC was already dead.

Take a closer look at AH1014 page45: 6.2.4 Sleep Mode

Application Hints

Re: TJA1043 application

The VBAT is not powered on in the constant power application scenario, and according to the reference application schematic, the local wake pin is pulled up to the VBAT through a resistor, so the wake pin is always high, so is it not used to control the wake up.

If the TJA1043 is not supplied with power at VCC via the CAN bus, can it receive a wake-up message from the CAN bus.

Re: TJA1043 application

INH 是上拉到VBAT的,通过外部设置STB/EN来控制TJA1043的状态控制INH的H/L,他是一直受控的因为VBAT没断电,比方说上电VBAT以后 TJA1043工作在sleep的模式,STB/EN都是floating的无法唤醒他,那么可以通过本地wake pin 或者Remote wake-up (via the CAN bus)唤醒 让INH 拉高从而让TJA1043 工作:

Any wake-up request, setting the Pwon flag or a LOW-to-HIGH transition on STB_N will
clear UVNOM and the timers, allowing the voltage regulators to be reactivated (at least until
UVNOM is set again).

guoweisun_0-1753941245889.pngguoweisun_1-1753941263720.png


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 06:16 PM
Updated by: