我使用S 3 2 G 399 A芯片,手动编译kernel,将L L C E 固件 和 驱动集成到根文件系统,手动加载L L CE CAN驱动报错,如下图。
请问是固件匹配问吗?还是缺少其他依赖?
期待回复!
Dear engineers
I am using the S 3 2 G 3 9 9 A chip, manually compiling the kernel, integrating the L L C E firmware and drivers into the root file system, and manually loading the L L C E CAN driver, but encountering an error, as shown below.
Is there a firmware compatibility issue or is there a lack of other dependencies?
Looking forward to your reply!
您好
从Log来看,可能是llce_can.ko依赖的其他module没有提前加载,您可以参考下BSPUM中的以下部分重新试一下
BR
Chenyin