2141813_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2141813_en-US

2141813_en-US

imx8mn-evk - yocto distro gatesgarth upgrade to styhead

Hi

I am in the process of upgrading our yocto distribution from gatesgarth to styhead.
When the upgrade is done we will be deploying the image via OTA using rauc.

From the above
1) We currently do not OTA the u-boot; therefore can we still use the gatesgarth u-boot-imx to boot the styhead kernel + dtb's?
2) Our current gatesgarth imx-boot is signed and looks for an authenticated kernel; if we authenticate the kernel using the same keys from gatesgarth; will the boot loader still be able to boot the styhead kernel?
3) Also please note from point 2 above the ui board has been fully locked down (efused and OTP fuse has already been applied)

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:12 AM
更新者: