2140795_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2140795_en-US

2140795_en-US

debug with multilink is ok,but fail after re-powerup

The K396 board I developed can be successfully pinged from my computer when running either the lwip_baremetal_s32k396 or lwip_FreeRTOS_s32k396 project using the Multilink debugger. However, after a power cycle, neither project can be pinged.

After changing the optimization level to none for the lwip_baremetal_s32k396 project, it can be pinged successfully without using the debugger. But for the lwip_FreeRTOS_s32k396 project, even after setting optimization to none, it still cannot be pinged without the debugger.

I added code to toggle an LED in vApplicationIdleHook, and it appears that the idle task is not being entered. What could be causing this issue?

Re: debug with multilink is ok

Just comment out PIT and that's fine. Thanks.

Re: debug with multilink is ok,but fail after re-powerup

Just comment out PIT and that's fine. Thanks.

Re: debug with multilink is ok,but fail after re-powerup

Hello @zhangzhixing ,

I experienced the same symptoms. Have you tried to disable PIT in device_init, as I mentioned in my update  Solved: lwip_FreeRTOS_s32k396' example project and failure - NXP Community ?

Best regards,

Pavel

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:16 AM
更新者: