2140433_zh-CN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2140433_zh-CN

2140433_zh-CN

imx8mp 路由器回环,导致NETDEV WATCHDOG复位,无法恢复

 您好,请问下我们的a板和b板同时接到交换机,然后a-b互ping,交换机由于误操作出现了环网(一个网线的两端都接到了交换机上),内核出现问题了(直接重启,或者debug卡死等),详细log在附件

[ 314.850236] ------------[ cut here ]------------
[ 314.854871] NETDEV WATCHDOG: ens3 (fec): transmit queue 0 timed out 3384 ms
[ 314.861910] WARNING: CPU: 0 PID: 15 at net/sched/sch_generic.c:525 dev_watchdog+0x234/0x23c
[ 314.870271] Modules linked in:
[ 314.873329] CPU: 0 PID: 15 Comm: ksoftirqd/0 Not tainted 6.6.3-g9d3450dbcab9-dirty #71
[ 314.881246] Hardware name: NXP i.MX8MPlus EVK board (DT)
[ 314.886555] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 314.893516] pc : dev_watchdog+0x234/0x23c
[ 314.897528] lr : dev_watchdog+0x234/0x23c
[ 314.901538] sp : ffff8000823e3c20
[ 314.904850] x29: ffff8000823e3c20 x28: 0000000000000100 x27: ffff8000823e3cd0
[ 314.911989] x26: ffff8000820d69c0 x25: 0000000000000d38 x24: ffff8000820d6000
[ 314.919128] x23: 0000000000000000 x22: ffff0000055503dc x21: ffff000005550000
[ 314.926266] x20: ffff00000589c400 x19: ffff000005550488 x18: 0000000000000006
[ 314.933404] x17: ffff8000821b62e8 x16: 0000000073e4d9ea x15: ffff8000823e3640
[ 314.940541] x14: 0000000000000000 x13: ffff8000820f0da0 x12: 0000000000000672
[ 314.947679] x11: 0000000000000226 x10: ffff800082148da0 x9 : ffff8000820f0da0
[ 314.954818] x8 : 00000000ffffefff x7 : ffff800082148da0 x6 : 80000000fffff000
[ 314.961956] x5 : 0000000000000000 x4 : 0000000000000000 x3 : 0000000000000000
[ 314.969093] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff00000412d880

i.MX8ULPLinux
Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 04:20 PM
Updated by: