2138225_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2138225_en-US

2138225_en-US

IW612 BT can't be brought up

I have IW612 (M2-MAYA-W271) on Verdin iMX95 EVK. It is  L6.12.3-1.0.0 image installed. Wifi works when moal driver and combo firmware are loaded.

 
modprobe moal mod_para=nxp/wifi_mod_para.conf



cat /lib/firmware/nxp/wifi_mod_para.conf

SDIW612 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=1
auto_ds=1
host_mlme=1
fw_name=nxp/sduart_nw61x_v1.bin.se
}
 

However, BT firmware don't seem to response.

modprobe btnxpuart
hciconfig hci0 up

[  147.824667] Bluetooth: hci0: Setting baudrate failed (-110)
[  149.840797] Bluetooth: hci0: Setting wake-up method failed (-110)
[  151.856817] Bluetooth: hci0: Setting Power Save mode failed (-110)
[  152.880918] Bluetooth: hci0: FW already running.
[  154.928780] Bluetooth: hci0: Opcode 0x0c03 failed: -110
[  167.824775] Bluetooth: hci0: Setting baudrate failed (-110)
[  169.840909] Bluetooth: hci0: Setting wake-up method failed (-110)
[  171.856888] Bluetooth: hci0: Setting Power Save mode failed (-110)
[  173.872779] Bluetooth: hci0: Setting baudrate failed (-110)

I tried the combo firmware together with open source HCI UART driver hciattach /dev/ttyLP4 any 115200 flow  with no luck. 

Do you have any idea how to enable BT? Thanks.


Re: IW612 BT can't be brought up

Dear @Benjamin_Hu ,


>>So is it fine that BT_15.4_RST is always high even during power reset?

In theory, this mod should work fine.

Because you said," It results in floating W_DISABLE2 and 1.7V on BT_15.4_RST signal".

When power on, the module should have an internal Power On Reset, don't need to control the reset via software.


Regards,

weidong




Re: IW612 BT can't be brought up

Thanks @weidong_sun 

U-blox module baud rate is 115200. I tried both 115200 and 3M in device tree. But it made no difference.

It may have something to do with the unconnected W_DISABLE2 on M.2 connector. There is a level-shifter on the U-blox module, mapping W_DISABLE2 to BT_15.4_RST of IW612. It will reset Bluetooth as well as 802.15.4 radio as long as it is asserted. Since it is unconnected, the host can't reset it.

Benjamin_Hu_0-1753262731153.png

However, there is also an I2C GPIO expander on the U-Blox modue. One GPIO from expander connects to BT_15.4_RST, too. The host is capable to reset BT and 802.15.4 via the I2C on M.2 connector regardless W_DISABLE2. Unfortunately, the I2C is also unconnected on the M.2 connector, meaning the host can not manipulate the expander. It results in floating W_DISABLE2 and 1.7V on BT_15.4_RST signal. 

So is it fine that BT_15.4_RST is always high even during power reset?

Re: IW612 BT can't be brought up

Dear @Benjamin_Hu ,


Because i.MX95-EVK of NXP version has not released to Mass Market yet, I don't have the schematic on my hand.  I checked your wifi module, it is M.2 card, so you should use it on M.2 KEY E connector.

I checked Linux release note of L6.12.3_1.0.0:

===============

Supports the NXP SDIO IW612 (tested with Murata LBES5PL2EL) on i.MX 93 and
i.MX 95 15x15 EVK.

===============

It is Murata 2EL M.2 module. Maybe there exists a little difference between these 2 M.2 modules . You can try like this:

Check if W_DISABLE1 & W_DISABLE2 on M.2 connector are both pulled up to HIGH, if not, pull up them to HIGH, please !  or drive 2 GPIOs connected to these 2 PINs to output HIGH.


[Addition]

You also need to confirm if the default baud rate is 3M with u-blox.  My M.2 2EL module's default baud rate is 115200.


Try it, please!

Thanks!
Regards,

weidong



Re: IW612 BT can't be brought up

It is 'fw-init-baudrate=3000000 ' by default in device tree.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 06:22 PM
Updated by: