2138005_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2138005_en-US

2138005_en-US

Sboot FCCU Ncf Tests - Alarm Timeout Enable

Hi, 

While testing Sboot FCCU NCF tests, one of the tests is getting failed due to alarm timeout disabled. Its not available in Emecm module. 

Could you mention where exactly it can be configured?

Regards, 
Irshad

GoldVIPRe: Sboot FCCU Ncf Tests - Alarm Timeout Enable

Hello, @Irshad2225 

Thanks for your confirmation.

The CMU_SAFETY_CORES_ERROR is related to the CMU_FC checking, I have checked the FCCU settings in eMcem, it is related to the fault_28, may I know if you have correctly set it via the eMcem?


BR

Chenyin

Re: Sboot FCCU Ncf Tests - Alarm Timeout EnableHi Chenyin,

SAF version: SW32G_SAF_2.0.2_QLP01_D2410
I have enabled only CMU_SAFERY_CORES_ERROR as R3 for test configuration.


Re: Sboot FCCU Ncf Tests - Alarm Timeout Enable

Hello, @Irshad2225 

Thanks for your post.

May I know which version SAF is used on your board? which test failed?


BR

Chenyin

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-20-2025 04:42 PM
更新者: