2134738_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2134738_en-US

2134738_en-US

how much i set tempSense Voltage supply?

i am using s32k344. i wanna use tempSense in mcu. 


how much i set tempSense Voltage supply?


if i set 0x15, is that mean is 1.5V?

Re: how much i set tempSense Voltage supply?

Hi@rlaxortn

I have already answered all of these in your previous questions.

if i set 0x15, is that mean is 1.5V?, the answer is yes,


But this value is not set randomly.

I suggest you read Chapter 85 Temperature Sensor in the data sheet .

Senlent_0-1752654010118.png


Re: how much i set tempSense Voltage supply?

Hi@rlaxortn

Just to correct myself, there were some errors in my answer.

The data format used was S11.4.

Therefore, the actual value = original 16-bit signed number ÷ 16


For example:

1.0x15 = 21 / 16 = 1.3125V

2.0x35 = 53 / 16 = 3.3125V

3.0x50 = 80 / 16 = 5V

Tags (1)
No ratings
Version history
Last update:
‎07-15-2026 02:28 AM
Updated by: