2130352_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2130352_en-US

2130352_en-US

error flashing vglite demo on rt1160

When I flash any vglite SDK examples onto my rt1160, nothing shows on screen. Furthermore, any subsequent attempts to flash another project onto the board gives the following error:


Executing flash operation 'Program' (Program file into flash: evkmimxrt1160_fbdev_freertos_cm7.axf) - Tue Jul 08 14:40:37 EDT 2025
Checking MCU info...
Scanning for targets...
Executing flash action...
LinkServer RedlinkMulti Driver v25.3 (Mar 25 2025 18:39:17 - crt_emu_cm_redlink build 945)
(  0) Reading remote configuration
Wc(03). No cache support.
Found chip XML file in /home/tzhuang/.workspaces/tmp-june-11/evkmimxrt1160_fbdev_freertos_cm7/Debug/MIMXRT1166xxxxx.xml
(  5) Remote configuration complete
Reconnected to existing LinkServer process.
============= SCRIPT: RT1160_connect_M7_wake_M4.scp =============
RT1160 Connect M7 and Wake M4 Script
DpID = 6BA02477
APID = 0x84770001
Setting M4 spin code
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Setting M4 clock
Error: Wire Ack Fault - target connected?
Resetting M4 core
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
Error: Wire Ack Fault - target connected?
View cores on the DAP AP
DpID = 6BA02477
============= END SCRIPT ========================================
Probe Firmware: DAPLink CMSIS-DAP (ARM)
Serial Number:  02440000020b6f0900000000000000000000000097969905
VID:PID:  0D28:0204
USB Path: /dev/hidraw1
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
connection failed - Nn(05). Wire ACK Fault in DAP access.. Retrying
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
Using memory from core 0 after searching for a good core
Failed on connect: Nn(05). Wire ACK Fault in DAP access
Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: 
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
Debug bus selected: MemAp 0
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
(100) Target Operation Failed
error closing down debug session - Nn(05). Wire ACK Fault in DAP access
Unable to perform operation!
Command failed with exit code 1

 The issue can be fixed by putting the board into SDP mode and serially flashing a working project. However, flashing any vglite demo puts the board into a bad state again.

The following demos work for me (with the expected output on my display):

  • evkmimxrt1160_fbdev_freertos_cm7
  • evkmimxrt1160_iled_blinky_cm7
  • evkmimxrt1160_mipi_dsi_compliant_test_cm7

The following demos put the board into a bad state:

  • evkmimxrt1160_clock_freertos_cm7
  • evkmimxrt1160_cube_freertos_cm7
  • evkmimxrt1160_tiger_freertos_cm7
Re: error flashing vglite demo on rt1160

Hi @tzhuang,

It seems to be an issue about the SDRAM configuration not being enabled in the flash build configuration. Please add the symbol definition for XIP_BOOT_HEADER_DCD_ENABLE=1 or XIP_BOOT_HEADER_XMCD_ENABLE=1 and try to build and flash the image again. For more information on what these symbol definitions do, please look at Table 3 of the following AppNote: How to Enable Debugging for FLEXSPI NOR Flash


Re: error flashing vglite demo on rt1160

Hi @tzhuang,

I was able to recreate the issue on my side. I tested a vglite example with SDK 2.16.000 and it worked fine. Then I changed to the latest SDK (v25.06.00) and I get a Wire ack fault immediately after flashing the image. My hypothesis is that something changed from SDK 2.xx to 2x.xx that broke the vglite examples.

I have reported this issue internally to the SDK team and will come back as soon as I receive a response.

Thanks for reporting this issue!

BR,
Edwin.

Re: error flashing vglite demo on rt1160I should also add that my colleague was able to get the vglite demos running on the same board using an older version of the IDE with SDK 2.15.00Re: error flashing vglite demo on rt1160Update: I also tried 25.06 for both the IDE and SDK and ran into the same issue.Re: error flashing vglite demo on rt1160Forgot to tag you in my response in case you missed it.Re: error flashing vglite demo on rt1160

Hi @tzhuang,

What SDK version are you using? Are you using VS Code extension or standalone MCUXpresso? If standalone, what version are you using?

标记 (1)
无评分
版本历史
最后更新:
‎11-22-2025 08:49 AM
更新人: