Hello.
I use RTD400 and SPD105, and the development board is the S32K312 144P development board
I added the FCCU module to the tested UART+DMA program without making any Settings. Even if the header file is not referenced and the FCCU part is not initialized in the code, the program will die at Clock_Ip_SetWaitStates
I added the uart module normally in the tested SPD module program (including RAM and flash injection errors), and then added the DMA module without making any Settings. Even if the header file and the initialization Fdma part are not referenced in the code, the program will still be in the function Clock_Ip_SetWaitStates(); Then it enters a hardware error interrupt.
I uploaded the code of UART+DMA without adding the FCCU module, and it can run normally. However, after adding it, there will be a hardware error in the clock initialization program. What could be the reason for this and how can this problem be solved?
I encountered a similar problem. It works when I use UART Interrupt mode of S32K312, but it enter HardFault_Handler(), when I running Lpuart_Uart_Ip_AsyncSend() or Lpuart_Uart_Ip_AsyncReceive() after Dma_Ip_Init() and Rm_Init().
Can anybody help me?
Hi@Neo1096
Sorry, we cannot support IAR, you can refer to the link file we provide to modify it.
Could you provide the icf file? I need to use it in IAR
Hi@Neo1096
We found the cause of the problem.
This is because of the configuration problem of the link file provided by S32 DS.
We replaced the link file in the SPD package with that in S32 DS, and this problem can be solved.
So please refer to the link file in the attachment for further testing.
Hi@Neo1096
The internal team has reproduced the problem and is currently eliminating possible causes.
Update time : 7/23/2025.
I haven't received a response from the internal forum yet, thank you for your patience.
Update data:15/7/2025.
I haven't received a response from the internal forum yet, thank you for your patience.
Update data:7/7/2025.
Hi@Neo1096
I pushed again this morning, but I haven't received any response from the internal forum yet.
This may be a bug, I need to confirm with the design team if I have overlooked something.
The current situation is that as long as I add the DMA module, it will enter hardfalut when initializing the clock.
I have tested it in different versions and the results are the same.
I added some code in exceptions.c under the Startup_Code folder, mainly to handle the hardware errors caused by error injection. The other parts remain unchanged.
I encountered your problem when testing the project "S32K312_SPD104_DMA_UART" you provided.
I haven't found the reason yet, but in theory, if your settings are the same as "S32K312_SPD104", there shouldn't be such a problem.
I will try to modify your code in "S32K312_SPD104" tomorrow.
It will take some time, and you may have modified the startup file.
The code I uploaded before can run. Adding the FCCU module separately will cause the operation to fail.
I re-uploaded two copies of the code.
A file that can run correctly tests RAM and FLASH injection errors based on the SPD104 version. (S32K312_SPD104)
Another one cannot run correctly. It is to add the DMA+UART part additionally in the previous code, which will be in Clock_Ip_SetWaitStates(); Enter the hardware interrupt (S32K312_SPD104_DMA_UART)
Please have a look. Thank you.
Hi@Neo1096
First,I tested the project you provided, and I did not encounter the problem you mentioned. Can you provide more information and whether some changes are needed?
Secondly, the SPD version corresponding to 4.0.0 P24 should be 1.0.4. You can try to install version 1.0.4 and try again