on s32k324, when we change clock settings from 160Mhz PLL to 48Mhz FIRC, the GPIO does not work anymore.(all gpio, not any specific pin)
we use RTD MCAL API
We found we have to call Mcu_Init()
Hi
There is RTD example Mcu_Example_S32K344 which switch clock settings by Mcu_InitClock API. Have you test it?
Did you enable the clock of SIUL2 in Clocks Tool?
Mcu_InitClock ClockConfig.png
If it still doesn't work, please send me a simplified test project.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------