2095090_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2095090_en-US

2095090_en-US

In the design of GUIder v1.8.0, there is an inconsistency between the interface design, the simulator display and the actual control display position of the microcontroller

In the design found to appear in the middle of the large font simulator display effect will be adjusted downward, microcontroller display will be adjusted upward using the font is their own imported bansnschrift, in fact, the text controls are the existence of positional deviation

批注 2025-05-12 112316.png批注 2025-05-12 112316.png

_0-1747020315218.jpeg_0-1747020315218.jpeg


Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题

Any results, please? I've been having this problem a lot.I don't know what to do with it.

Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题

hi, @Harry_Zhang
I have uploaded the file to the attachment as you provided.
The details of the problem and where I think the problem occurs are mentioned in the previous reply: problem reproduction and causes.
If you have a solution, please kindly contact me!
Looking forward to your reply!

Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题

Hello @Harry_Zhang

How should I share my project with you
Actually I have almost pinpointed where the problem is
The inconsistency between the effect on the microcontroller and the simulator is my problem The inconsistency between the simulator and the interface design is due to the problem with the baseline offset in the generated font file, which is different from that of the interface design but I don't know how to correct the situation from my side
If you can, could you please provide me with an email address, I will copy the project for you to reproduce and add some notes.
I look forward to your reply!
How to reproduce it:
Add the border of the label and make the font as big as possible, so that you can see the y-axis offset of the font in the label box.

_0-1747196923328.png_0-1747196923328.png

Possible reasons for this problem:
The font position offsets during interface design are different from the emulator font offsets and may appear in this font file

_1-1747197180404.png_1-1747197180404.png


Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题

Hi @陈宇 

Can you share your project? I want to reproduce this issue.

BR

Harry

Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题

_0-1747031819187.png_0-1747031819187.png

I use the official built-in Song test and this problem also occurs, the white places are where I use the container to mark the positional relationship between the controls

Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题I found that this happens when I use my own added font file ttf This does not happen when I use the official built-in font files: plain English and numeric
The problem is localized to the font file that I added in?
But I added the official ttf file, and I don't know how to solve the problem of inconsistency between the design effect, the simulator effect and the actual display effect of the microcontroller.
If you have a solution for this problem, please provide it to me.
Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题

Hi @xiaohuihui

We'll address this in a future version.

If you need a large font size, it is recommended to adjust the offset according to the actual screen display to ensure that the final screen can be displayed properly.

BR

Harry.

Re: 在GUIder v1.8.0设计中,出现界面设计、模拟器显示和单片机实际控件显示位置不一致的问题There is no solution at the moment I don't know if there is an official update
I'm currently looking at the actual effect to adjust the position of the controls
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-26-2026 04:40 AM
更新者: