This article describes how to evaluate ULPCD feature together with PN7642 EVK (OM27642EVK) and NFC Cockpit.
OM27642EVK does not required any HW changes for ULPCD (**). User is only required to change the following settings in EEPROM (disable DC-DC converter).
Address: 0x0000 (Secure_Lib_Config)
Value: 0x21
Reset the board after writing the value.
Tomas_Parizek_0-1745904468298.png
**Note: To ensure an accurate and reliable ULPCD evaluation—particularly for ULPCD current measurements. We strongly recommend implementing the following hardware modifications on the OM27642EVK.
PN7642_MB.png
Note: New revision of the board already have R4=DNP, R8=0Ω. Kindly check this on your board.
PN7642_EEPROM_ULPCD.png
Once the required ULPCD settings is set (Guard times, Threshold....). Then User has to perform "Reads HF Attenuator". Make sure that the "HF Attenuator" option is checked.
As written above, the value must not be 0x00. If so, increase VDDPA.
For OM27642EVK, the RSSI value for unloaded antenna is typically around 1400dec - 1600dec.
User can enter the ULPCD mode. The board will again be connected once the load change is detected (e.g. NFC card or smartphone in the antenna proximity).
Tomas_Parizek_0-1782466647959.png