"fatal error: Spi.h: No such file or directory" error occurs when building /BMS_K322_M7_0/RTD/include/sbc_spi_external_access.h
RTD Information:
SW Version: 3.0.0
Build Version: S32K3_RTD_3_0_0_P07_D2306_ASR_REL_4_7_REV_0000_20230629
SBC_FS26 Driver Info:
SW Version: 3.0.0
Build Version: S32K3_RTD_3_0_0_P07_D2306_ASR_REL_4_7_REV_0000_20230629
We are not using AUTOSAR, so we are not using MCAL.
Hi
Since you are using non-AUTOSAR, you should not use Spi.h. Try to add USE_IPV_LPSPI in Preprocessor:
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------