I was using OM15080-JN5189, and the firmware was the factory firmware. When conducting the zgwui test with the nxp tool, no matter what instructions were sent, there was no response. I performed the operation according to the ttug.pdf file.May I ask how I should configure it or what firmware to flash?2025-04-24_164053.png
Thank you for your reply. I can use it now, but I can't find the file JN-AN-1244. Could you please give me the relevant link?
liushuiwuqing_0-1745909577846.png
Hello,
Hope you are doing well.
Could you clarify what the "ttug.pdf" refers to? What is the process that you did to program the devices? Is there a specific guide or document you are following?
I would recommend checking out the following documents:
DK6 Production Flash Programmer User Guide included in the SDK files under this path: SDK\docs\DK6-UG-3127-Production-Flash-Programmer
Zigbee 3.0 IoT Control Bridge UserGuide under the path JN-AN-1247.zip\JN-AN-1247\Doc
Best Regards,
Ana Sofia.