2080735_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2080735_en-US

2080735_en-US

iMxRT1040 Boot FlexSPI and DQS

Hi,

I have a problem with my configuration to fit all the required peripherals.

I plan to use external Quad SPI NOR Flash with no Strobe. (as the EVK).

I need to use : CCM.CLKO1 [J4] and CCM.CLKO2 [J1].

I need one FlexSPI (for ext Flash) and one uSDHC for SdCard.

The 2 clocks outputs prevent me from using uSDHC1.

Then, I have to use uSDHC2 for the SdCard that has the CMD signal on [M4].

The [M4] pin is shared with FLEXSPI.A_DQS.

What's the best way to use SdCard and boot on FlexSPI ?

Can I boot easily on FLEXSPI2.A ? or should I use FlexSPI1.A with internal loopback Strobe ?

Thanks in advance,






Re: iMxRT1040 Boot FlexSPI and DQS

Hi @jfz_arturia ,

Thank you for your interest in the NXP MIMXRT product, I would  like to provide service for you.


Question: Can I boot easily on FLEXSPI2.A ?

Answer: No, You can't. 

In IMXRT1040RM reference manual, You can see that NOR Flash can only be  boot on FlexSPI1

mayliu1_0-1744786079793.pngmayliu1_0-1744786079793.png


Question: or should I use FlexSPI1.A with internal loopback Strobe ?

Answer:  You can use this mode, but the max Frequency of operation is limited to 60MHz if you use this mode .

https://www.nxp.com/webapp/Download?colCode=IMXRT1040RM


mayliu1_1-1744786297566.pngmayliu1_1-1744786297566.png

https://www.nxp.com/docs/en/data-sheet/IMXRT1040CEC.pdf


mayliu1_2-1744786431211.pngmayliu1_2-1744786431211.png

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 09:31 PM
Updated by: