Hi,
I'm developing software based on S32K3xx Demo app.
In order to Update Secure Life Cycle, ADKP need to be is programmed.
After ADKP is programmed, the secure debug feature is enabled.
I got 2 questions:
Thanks a lot.
Here are two screenshots from the manual:
So, it is mandatory to configure ADKP when advancing the life cycle and it's not possible to disable secure debug because it's programmed to OTP.
Regards,
Lukas