2069257_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2069257_en-US

2069257_en-US

Inquiry About MCAL BSP Support for MPC5775B
Dear NXP Support Team,
 
 
We recently purchased the MPC5775B BMS and VCU Reference Design (RDVCU5775EVM) under the assumption that a supporting MCAL BSP is available for the MPC5775B microcontroller. However, I was unable to find any MCAL package on your website for this specific controller.
Could you kindly provide guidance on where I can obtain the MCAL BSP for this MCU? If it is not publicly available, please let me know the process to access it.
Looking forward to your response.
Re: Inquiry About MCAL BSP Support for MPC5775B

Thanks for all the responses so far, I am good with tres os studio installation and supporting MCAL package for MPC5775B.Iam very much newbie to the tool and trying to configure pins, directions and drivers. The tool which I have installed is EB tresos 21.0. I am trying to configure the pins for SPI driver. Can someone help me out how to kick start? upon browsing I am supposed to configure port ID and direction. But I don't find any option to configure such. Kindly help me out with some genuine tutorial. Also will there be any kind of manual/input sheet for configuring drivers like SPI, CAN, NVM for the given product RDVCU5775EVM. 

Lasya_0-1743661590809.png



Re: Inquiry About MCAL BSP Support for MPC5775B

Hello,

When it is not suggested to use SDK how can I apply RTOS features now? Can I only use only RTOS feature of SDK or what would be the best approach?

Well, if you want AUTOSAR spec OS, then you have to go to third party, like Elektrobit or Vector.

As you can see on our web AUTOSAR OS is not available form NXP, as we were not participating on development of it.

petervlna_0-1743575359948.png

You can use FreeRTOS, but it is not AUTOSAR compliant.

Best regards,

Peter



Re: Inquiry About MCAL BSP Support for MPC5775B

Thanks for all the provided solutions. It worked and now I am able to configure the drivers for MCAL.

But the only component I am concerned is about RTOS (Free RTOS). When it is not suggested to use SDK how can I apply RTOS  features now? Can I only use only RTOS feature of SDK or what would be the best approach?

Re: Inquiry About MCAL BSP Support for MPC5775B

Hello,

Does the Power Architecture SDK support integration with MCAL?

SDK is not autosar complaint. So I suppose such would not be possible. Also I would not recommend it, especially when MCAL is free of charge.

https://www.nxp.com/docs/en/fact-sheet/S32SDKFS.pdf

Is there an official MCAL package available for MPC5775B? If so, where can I download it?

Yes, You can find it directly at the web of the MPC5775B. As I have expressed earlier.

petervlna_0-1743404118892.png

What is the recommended approach to integrate MCAL with EB tresos Studio for AUTOSAR compliance?

Simply install it. MCAL is only software package supported by EB tresos configuration GUI.

Not sure what you want to integrate into the GIU.

Best regards,

Peter

Re: Inquiry About MCAL BSP Support for MPC5775BHello , Please help me with above questionsRe: Inquiry About MCAL BSP Support for MPC5775B


When trying to extract the MCAL safety pack files, it is asking to browse for ".lic" file which is unknown. Could you please help me in locating the .lic file

Lasya_1-1743156923709.png



Re: Inquiry About MCAL BSP Support for MPC5775BAlright!! Thanks. Kindly help me with my other question as wellRe: Inquiry About MCAL BSP Support for MPC5775B

hello,

Hmm, that's weird.

You will need to get in touch with Elektribit support as Tresos is not NXP product and we do not have knowledge on such issues.

Best regards,

Peter



Re: Inquiry About MCAL BSP Support for MPC5775B

Kindly help me with these questions also please

Re: Inquiry About MCAL BSP Support for MPC5775B

I am doing the same . I entered the activation code and also able to acheive succesful activation. When I open the tresos studio it always for a license key which is not findable for me.

Lasya_0-1743146994567.pngLasya_1-1743147039244.png

Kindly help me with the solution

Re: Inquiry About MCAL BSP Support for MPC5775B

Hello,

Hmm, the license file is generated from license admin app.

petervlna_0-1743146416527.png

Just enter the code and that is it:

petervlna_1-1743146458987.png

Best regards,

Peter



Re: Inquiry About MCAL BSP Support for MPC5775B

Hello,

Yes, those 2 devices share the same BSP.

Best regards,

Peter

Re: Inquiry About MCAL BSP Support for MPC5775BHello,

I am working with the MPC5775B microcontroller and have imported the Power Architecture SDK for this device. I now need a compatible MCAL package to configure drivers and integrate with an RTOS.

Could you please confirm:

Does the Power Architecture SDK support integration with MCAL?

Is there an official MCAL package available for MPC5775B? If so, where can I download it?

What is the recommended approach to integrate MCAL with EB tresos Studio for AUTOSAR compliance?

Any guidance or documentation references would be greatly appreciated.

Thanks in advance!
Re: Inquiry About MCAL BSP Support for MPC5775B

Hello, I obtained a product key for tresos studio . I activated the license but not able to obtain the .lic file ad now not able to access the tresos studio . Kindly help me

Re: Inquiry About MCAL BSP Support for MPC5775B

Thanks for the reply.

Re: Inquiry About MCAL BSP Support for MPC5775B

Thanks for the quick reply,

Are you sure the MCAL for the MPC5777C meets our requirements for the MPC5775B? The MCU series number is different.

Re: Inquiry About MCAL BSP Support for MPC5775B

Hello,

Hmm seems like the MPC5777C is missing in the links list

https://www.nxp.com/design/design-center/software/automotive-software-and-tools/autosar/autosar-4-0-...

petervlna_0-1743062576911.png

MPC5775B/E and MPC5777C use the same package. As MPC5775 is only derivative of MPC5777C.

petervlna_1-1743062646841.png

Best regards,

Peter



Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 09:45 PM
Updated by: