We are using i.MX 8X with analog video via ADV7280A-M MIPI CSI-2 and Yocto Linux Scarthgap and Qt 6.8.2.
The following works:
gst-launch-1.0 v4l2src device=/dev/video2 ! video/x-raw,width=720,height=567,framerate=25/1 ! autovideosink
But the equivalent does not work from Qt (gst_parse_element_make: no element "video").
Therefore am trying:
gst-launch-1.0 -vvv v4l2src device=/dev/video2 ! rawvideoparse width=720 height=576 format=yuy2 ! autovideosink
However that fails with
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory.
The full output is:
Setting pipeline to PAUSED ...
error: XDG_RUNTIME_DIR is invalid or not set in the environment.
error: XDG_RUNTIME_DIR is invalid or not set in the environment.
EGL: Warning: No default display support on wayland
EGL: Warning: No default display support on wayland
Pipeline is live and does not need PREROLL ...
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstKMSSink:autovideosink0-actual-sink-kms: display-width = 1280
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstKMSSink:autovideosink0-actual-sink-kms: display-height = 768
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)3840, height=(int)2160, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstRawVideoParse:rawvideoparse0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)3840, height=(int)2160, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory.
Additional debug info:
/usr/src/debug/gstreamer1.0-plugins-good/1.24.0.imx/sys/v4l2/gstv4l2src.c(955): gst_v4l2src_decide_allocation (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
Buffer pool activation failed
Execution ended after 0:00:00.043197264
Setting pipeline to NULL ...
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.
Additional debug info:
/usr/src/debug/gstreamer1.0/1.24.0.imx/libs/gst/base/gstbasesrc.c(3175): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason not-negotiated (-4)
Freeing pipeline ...
Thank you
-- Peter
Hi @joanxie,
GST_DEBUG=3 gst-launch-1.0 -v v4l2src num-buffers=5 device=/dev/video0 ! video/x-raw,format=GRAY8,depth=8,width=1280,height=800 ! videoconvert ! jpegenc ! multifilesink location=ar0144_mono_image.jpg
issue is
Starting GStreamer pipeline...
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
0:00:00.244283375 784 0xffffb4000b70 WARN v4l2 gstv4l2object.c:5023:gst_v4l2_object_get_crop_rect:
0:00:00.244416875 784 0xffffb4000b70 WARN v4l2 gstv4l2object.c:5230:gst_v4l2_object_probe_caps:
New clock: GstSystemClock
0:00:00.246845250 784 0xffffb4000b70 WARN v4l2 gstv4l2object.c:5023:gst_v4l2_object_get_crop_rect:
/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, format=(string)GRAY8, depth=(int)8, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, format=(string)GRAY8, depth=(int)8, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressie
/GstPipeline:pipeline0/GstVideoConvert:videoconvert0.GstPad:src: caps = video/x-raw, format=(string)GRAY8, depth=(int)8, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progre
/GstPipeline:pipeline0/GstJpegEnc:jpegenc0.GstPad:sink: caps = video/x-raw, format=(string)GRAY8, depth=(int)8, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive
/GstPipeline:pipeline0/GstVideoConvert:videoconvert0.GstPad:sink: caps = video/x-raw, format=(string)GRAY8, depth=(int)8, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)proge
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, format=(string)GRAY8, depth=(int)8, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progresse
0:00:00.253795500 784 0xffffb4000b70 WARN v4l2 gstv4l2object.c:5023:gst_v4l2_object_get_crop_rect:
0:00:00.253877250 784 0xffffb4000b70 WARN v4l2 gstv4l2object.c:5023:gst_v4l2_object_get_crop_rect:
0:00:00.259326750 784 0xffffb4000b70 ERROR v4l2bufferpool gstv4l2bufferpool.c:721:gst_v4l2_buffer_pool_streamon:
0:00:00.259393750 784 0xffffb4000b70 ERROR bufferpool gstbufferpool.c:572:gst_buffer_pool_set_active:
0:00:00.259435250 784 0xffffb4000b70 WARN v4l2src gstv4l2src.c:955:gst_v4l2src_decide_allocation:
0:00:00.259461750 784 0xffffb4000b70 WARN v4l2src gstv4l2src.c:955:gst_v4l2src_decide_allocation:
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory.
Additional debug info:
/usr/src/debug/gstreamer1.0-plugins-good/1.24.0.imx/sys/v4l2/gstv4l2src.c(955): gst_v4l2src_decide_allocation (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
Buffer pool activation failed
0:00:00.259690375 784 0xffffb4000b70 WARN basesrc gstbasesrc.c:3395:gst_base_src_prepare_allocation:
Execution ended after 0:00:00.015445250
Setting pipeline to NULL ...
0:00:00.259771000 784 0xffffb4000b70 WARN basesrc gstbasesrc.c:3175:gst_base_src_loop:
0:00:00.259796500 784 0xffffb4000b70 WARN basesrc gstbasesrc.c:3175:gst_base_src_loop:
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.
Additional debug info:
/usr/src/debug/gstreamer1.0/1.24.0.imx/libs/gst/base/gstbasesrc.c(3175): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason not-negotiated (-4)
Freeing pipeline ...
GStreamer command finished.
For completeness, this thread's original issue was solved using capsfilter, rather than rawvideoparse:
player.source = "gstreamer-pipeline: v4l2src device=/dev/video2 ! capsfilter caps=video/x-raw,width=720,height=480,framerate=25/1"
That does then have an intermittent SIGSEGV in gst_v4l2_object_fill_format_list, when used with Qt, but guess that is another issue.
Hi @Ahmed230, your message has a very large font size, making it hard to read.
This thread is about ADV7280A-M (NTSC/PAL) working ok with: "! video/x-raw...", but not with: "! rawvideoparse..."
Your message is about AR0144 image sensor not working with: "! video/x-raw".
Different topic. Best to start a new post, and Ctrl+Shift+V to paste just the text, without the large font.
Also replace the $NUMBER_OF_PIC, $VID_DEVICE, $FRAME_SIZE with the actual values.
My issue is with nxp 6.6.36 kernel for camera ar0144 on iMX8MM board to capture image or videos
this time, what print error information you get? I compare the bsp 6.6 with bsp 5.10, bsp 6.6 remove the code from 5.10 based this patch , did you try 5.10 bsp?
https://github.com/nxptest/linux-imx/commit/4f87610383a0f365ee0c68d9354ddcf099240144
PS @joanxie
Re:
0:00:00.518350875 427 0xffff80000b70 WARN v4l2 gstv4l2object.c:5023:gst_v4l2_object_get_crop_rect:v4l2src0:src Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument
this is because mxc_isi_cap_g_selection() is being called with:
type 1 V4L2_BUF_TYPE_VIDEO_CAPTURE and
target 1 V4L2_SEL_TGT_CROP_DEFAULT (and target 2 V4L2_SEL_TGT_CROP_BOUNDS)
but is only expecting type V4L2_BUF_TYPE_VIDEO_OUTPUT or V4L2_BUF_TYPE_VIDEO_OUTPUT_MPLANE
https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/drivers/staging/media/imx/imx8-isi-cap.c#L1164
Adding handling for those makes the warning go away.
(But then mxc_isi_cap_s_fmt_mplane is called
and for some reason fmt changes from RGB565 720x480 to YUYV-16 3840x2160 anyway).
Hi @joanxie
We are using Yocto Scarthgap and linux-imx
uname shows 6.6.52
We forked from linux-imx after this commit:
https://github.com/nxp-imx/linux-imx/commit/e0f9e2afd4cff3f02d71891244b4aa5899dfc786
If I add debug to drivers/staging/media/imx/imx8-mipi-csi2.c mxc_csi2_get_sensor_fmt(), that shows
720 x 480.
Therefore am confused why
v4l2-ctl --get-fmt-video -d /dev/video2
shows 3840/2160
And wondering whether to implement VIDIOC_G_SELECTION or VIDIOC_CROPCAP somewhere for more consistency.
Thank you
-- Peter
what bsp version do you use? it seems the scale issue, that's why I asked you to test specific resolution, otherwise need to upscale to 3840, which would cause error
Hi @joanxie, thank you for replying.
v4l2-ctl -d /dev/v4l-subdev1 --set-standard PAL
Using "video/x-raw, width=720, height=480" works with gst-launch-1.0.
However the issue is that using video/x-raw in gstreamer-pipeline: in Qt 6.8.2 (QML MediaPlayer) fails:
ERROR GST_PIPELINE grammar.y:630:gst_parse_element_make: no element "video"
Under Qt (which uses playbin) video/x-raw is not recognised as an element, because it is a caps filter.
That is why I was trying to get a pipeline working without needing the video/x-raw caps filter in it...
Ok, just found that there is a capsfilter element, so using that explicitly instead:
player.source = "gstreamer-pipeline: v4l2src device=/dev/video2 ! capsfilter caps=video/x-raw,width=720,height=480,framerate=25/1"
That almost works from Qt. Shows video for a bit but then segfaults with:
1 format_cmp_func gstv4l2object.c 1276 0xffffd80668dc
2 g_slist_insert_sorted_real gslist.c 913 0xfffff604fab4
3 g_slist_insert_sorted gslist.c 964 0xfffff60504e0
4 gst_v4l2_object_fill_format_list gstv4l2object.c 1324 0xffffd8065a60
5 gst_v4l2_object_get_format_list gstv4l2object.c 1373 0xffffd8065f2c
6 gst_v4l2_object_probe_caps gstv4l2object.c 5212 0xffffd806ed34
7 gst_v4l2_object_get_caps gstv4l2object.c 5310 0xffffd806ef38
8 gst_base_src_default_query gstbasesrc.c 1373 0xffffd9219490
9 gst_pad_query gstpad.c 4228 0xffffd90ec24c
10 gst_pad_query_caps gstutils.c 3117 0xffffd913140c
11 gst_v4l2src_negotiate gstv4l2src.c 786 0xffffd8079a04
12 gst_base_src_negotiate_unlocked gstbasesrc.c 3490 0xffffd9213e9c
13 gst_base_src_loop gstbasesrc.c 2915 0xffffd9215e7c
14 gst_task_func gsttask.c 399 0xffffd9122090
15 g_thread_pool_thread_proxy gthreadpool.c 350 0xfffff605d780
16 g_thread_proxy gthread.c 831 0xfffff605cad8
17 start_thread pthread_create.c 447 0xfffff6730fc4
18 thread_start clone3.S 76 0xfffff67931cc
Will see what I can figure out.
Either way, am wondering:
v4l2-ctl --device /dev/video2 --all
gives mxc-isi-cap_v1 Width/Height: 3840/2160 ...
Guess because even though the ADV is only capable of 720 wide, the MIPI CSI-2 is capable of 3840.
This changes it, but only temporarily:
v4l2-ctl -d /dev/video2 -vwidth=720,height=480
It reverts back to 3840 when gstreamer is run without the capsfilter.
Seeing as on our i.MX 8X based board, the MIPI CSI-2 is hard wired to the ADV, and will only ever be used as 720 wide, is there any way of configuring it to stay at 720 wide, rather than 3840 wide? That would make it "just work" and simplify the gstreamer pipeline for Qt etc?
Thank you
-- Peter
what format do you set for the ADV7280, how about set the specific resolution in the pipeline? for example, video/x-raw, width=720, height=480, it seems the issue related to the crop, you can try to set the resolution and test again
https://github.com/GStreamer/gst-plugins-good/blob/master/sys/v4l2/gstv4l2bufferpool.c#L668
if (obj- >ioctl (pool- >video_fd, VIDIOC_STREAMON, &obj- >type) < 0)
goto streamon_failed;