HI NXP Teams
I am evaluating the I.MX95 for multi-camera and multi-display applications. Since two sets of MIPI-CSI are required simultaneously, DSI cannot be used for the display. I would like to know if the two 1x4 LVDS ports can output different display information separately? What is the supported bitrate and resolution?
poyuan
I understand the current status of the I.MX95. Can the two BOE WXGA LVDS panels on the EVK output different information? If I create my own adapter, can it output 1080P, 30FPS information?
Hello,
Please note that i.MX95 is still in pre-production stage so all information and specifications herein are subject to change without notice.
I.MX95 is capable of a 2x 4-lane or 1x 8-lane LVDS display interface capable of 1080p60 resolution.
On the EVK there is 2 combinations available either two single-channel LVDS-to-HDMI converter or two BOE WXGA LVDS panel.
Best regards/Saludos,
Aldo.