Hi,
We are using an NPU for an ML application, which requires Ethosu. However, our low-level application runs on an M33 core. We are trying to integrate it into the existing ethosu_rpmsg_app, but it already consumes a lot of memory. We need to increase the memory size from 128K to 256K. Please share the method to achieve this.
Memory Consumption of Demo example m33_sdk/boards/mcimx93evk/demo_apps/ethosu_apps_rpmsg -
Hello,
Yes you should
Regards
Hi,
So, should we consider that only 128KB of TCM is available? Is there no option to extend it from 128KB to 256KB?
Regards,
Gopal Sharma
Hello,
There is an issue with TCM and M33, previously posted here:
Regards