2060480_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2060480_en-US

2060480_en-US

After s32k144's can0 enables can fd, can1 and can2 become unusable?

Hello:

My environment is s32 ds, and I use PE to configure peripherals. All three cans are initialized in the code, but if I enable can0 fd in PE, the firmware cannot run after burning. If I do not enable can0 fd, the firmware can run. In addition, if I enable can0 fd but do not initialize can1 and can2, the firmware can also run.

The question I want to confirm is: if can0's fd is enabled, then can1 and can2 cannot be used?

Thanks!

Re: After can fd is enabled on can0 of s32k144, can1 and can2 become unusable?

Ok, thanks for confirming, I'll look for the reason!

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 02:12 PM
Updated by: