2060265_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2060265_en-US

2060265_en-US

Whether the code of KW38 and KW45 is common

I am using KW38 now, and the RAM of KW38 is not enough. As far as I know, many software of KW38 and KW45 are compatible, so whether the program of KW38 can be directly run on KW45? I just want to quickly replace it and test how much memory is needed, and verify how much RAM is needed first

Product: KW 37|38|39Re: Whether the code of KW38 and KW45 is commonOk, thank you for your answerRe: Whether the code of KW38 and KW45 is common

Hi

KW38 and KW45 are not pin compatible, there are some differences in Application structure and APIs used for each device. For development using a new board, and in order to avoid any issues related to the software, I would recommend checking on the Bluetooth Low Energy Application Developer’s Guide Chapter 9 to see how this structures are integrated; also, this document describes the most commonly used APIs and provides code examples applicable to KW45.


I would recommend using the SDK examples for KW45 as base for developing your application if you are trying to move to KW45.


Best Regards

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:55 PM
Updated by: