2057915_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2057915_en-US

2057915_en-US

Create frame buffer without hdmi device
  • Processor: iMX8M
  • System: Yocto with Wayland 

I would like to play video immediately after the system starts. However, I encounter a problem when the HDMI cable isn't connected during system startup. In this situation, a frame buffer isn't created, which is correct in the normal situation. I can't start playing such situation.  Is there any way to create a frame buffer with specified resolution without detecting the HDMI device? The approach should continue to play the video after connecting the cable on a compatible screen.

Graphics & Displayi.MX 8M | i.MX 8M Mini | i.MX 8M NanoLinuxMultimediaYocto ProjectRe: Create frame buffer without hdmi device

Hello,

Unfortunately no, for video to continue to be played needs a sink (display).

Best regards/Saludos,
Aldo.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 02:21 PM
更新者: