Messr NXP,
can you confirm that the products PCA9633DP2 and PCA9632DP2Z are perfectly interchangeable in existing boards without any FW intervention?
Hi Team,
I am using the PCA9632DP2Z to drive a 12V RGB LED. Since this IC operates at 5V, I have incorporated a transistor driver circuit. Kindly review the circuit below and share your feedback or suggestions
Hello Luigi,
Both devices support I2C communication with Fast-mode Plus (1 MHz) and share the same register structures with default settings. The slave address is also identical. So, I believe that no FW changes are necessary.
BRs, Tomas