2055571_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2055571_en-US

2055571_en-US

MIMXRT1064 spi

Hi, we got a MIMXRT1064-EVK board to develop an application that was done on a iMx8QM, an added feature this time is SPI, i used the b2b_master example to try to communicate with other boards (raspberry(raspi-os), arduino uno (arduino), esp8266(arduino)) but had no luck making the MIMXRT1064 work as master or slave in SPI.

By using an oscilloscope i noticed that the MIMXRT1064 doesn't output any clock in the SCK pin during transmission, there is no activity at all on any of the SPI pin of the arduino header. I tried with the given example and also by modifying it trying to make it work, any clue what could be the reason for the SPI not working?

Re: MIMXRT1064 spi

Solution: it was just a resistor issue, MIMXRT1064-evk doesn't come stock with the arduino header jumper resistors so i had to solder some 0402 0 ohm resistors in place, after this was done everything come back to a working status.

mimxrt1064.png

Re: MIMXRT1064 spi

this is the sligthly modified code of freertos_lpspi_b2b_master just to continously (time interval)  send a message on SPI.

/*
 * Copyright (c) 2013 - 2015, Freescale Semiconductor, Inc.
 * Copyright 2016-2019 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

/* FreeRTOS kernel includes. */
#include "FreeRTOS.h"
#include "task.h"
#include "queue.h"
#include "timers.h"

/* Freescale includes. */
#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "fsl_lpspi.h"
#include "fsl_lpspi_freertos.h"
#include "board.h"
#include "app.h"

/*******************************************************************************
 * Definitions
 ******************************************************************************/
#define TRANSFER_SIZE     (16U)    /*! Transfer dataSize.*/
#define TRANSFER_BAUDRATE (500000U) /*! Transfer baudrate - 500k */

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
/* LPSPI user callback */
extern uint32_t LPSPI_GetInstance(LPSPI_Type *base);

/*******************************************************************************
 * Variables
 ******************************************************************************/
lpspi_slave_handle_t g_s_handle;

uint8_t masterReceiveBuffer[TRANSFER_SIZE] = {0};
uint8_t masterSendBuffer[TRANSFER_SIZE]    = {0};
uint8_t slaveSendBuffer[TRANSFER_SIZE]     = {0};

SemaphoreHandle_t lpspi_sem;
/*******************************************************************************
 * Definitions
 ******************************************************************************/
/* Task priorities. */
#define master_task_PRIORITY (configMAX_PRIORITIES - 1)

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
static void master_task(void *pvParameters);

/*******************************************************************************
 * Code
 ******************************************************************************/
/*!
 * @brief Application entry point.
 */
int main(void)
{
    int i;

    /* Init board hardware. */
    BOARD_InitHardware();

    PRINTF("FreeRTOS LPSPI master example starts.\r\n");

    PRINTF("This example uses two boards to connect with one as master and anohter as slave.\r\n");

    PRINTF("Master and slave are both use interrupt way.\r\n");
    PRINTF("Please make sure you make the correct line connection. Basically, the connection is:\r\n");
    PRINTF("LPSPI_master -- LPSPI_slave\r\n");
    PRINTF("    CLK      --    CLK\r\n");
    PRINTF("    PCS      --    PCS\r\n");
    PRINTF("    SOUT     --    SIN\r\n");
    PRINTF("    SIN      --    SOUT\r\n");
    PRINTF("\r\n");

    /* Initialize data in transfer buffers */
    for (i = 0; i < TRANSFER_SIZE; i++)
    {
        masterSendBuffer[i]    = i % 256;
        masterReceiveBuffer[i] = 0;

        slaveSendBuffer[i] = ~masterSendBuffer[i];
    }

    if (xTaskCreate(master_task, "Master_task", configMINIMAL_STACK_SIZE + 64, NULL, master_task_PRIORITY, NULL) !=
        pdPASS)
    {
        PRINTF("Task creation failed!.\r\n");
        while (1)
            ;
    }
    vTaskStartScheduler();
    for (;;)
        ;
}

/*!
 * @brief Task responsible for master SPI communication.
 */
static void master_task(void *pvParameters)
{
    lpspi_transfer_t masterXfer;
    lpspi_rtos_handle_t master_rtos_handle;
    lpspi_master_config_t masterConfig;
    status_t status;

    LPSPI_MasterGetDefaultConfig(&masterConfig);
    masterConfig.baudRate = TRANSFER_BAUDRATE;
    masterConfig.whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;

    status = LPSPI_RTOS_Init(&master_rtos_handle, EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, LPSPI_MASTER_CLK_FREQ);
    if (status != kStatus_Success)
    {
        PRINTF("LPSPI master: error during initialization. \r\n");
        vTaskSuspend(NULL);
    }

    /*Start master transfer*/
    masterXfer.txData      = masterSendBuffer;
    masterXfer.rxData      = masterReceiveBuffer;
    masterXfer.dataSize    = TRANSFER_SIZE;
    masterXfer.configFlags = EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_SlaveByteSwap;

    for(int j=0; j<100; j++){
		status = LPSPI_RTOS_Transfer(&master_rtos_handle, &masterXfer);
		if (status == kStatus_Success)
		{
			PRINTF("LPSPI master transfer completed successfully.\r\n");
		}
		else
		{
			PRINTF("LPSPI master transfer completed with error.\r\n");
		}
		vTaskDelay(1000);
    }

    vTaskSuspend(NULL);
}

Re: MIMXRT1064 spi

note that communication from e to the other devices work, the problem is just with the MIMX board

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 10:06 PM
更新者: