2055522_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2055522_en-US

2055522_en-US

Minimum input voltage for edge capture

Hi,

In a KV4X, for a digital input, input voltage high is 0.7 x Vdd and input voltage low is 0.35 x Vdd.

Which are the minimum and maximum values for edge capture?

I have a sinusoidal signal of 200 mV peak in an input pin and I see that it is enough to detect falling/rising edges.

Thanks in advance



Re: Minimum input voltage for edge capture

I have found why edges were being detected with such a low signal.

Re: Minimum input voltage for edge capture

Hi @zorrotz,

Please maintain the edges of the captured signal between 0.7 x Vdd and 0.35 x Vdd in order to ensure a proper edge detection of the signal.


Re: Minimum input voltage for edge capture

I have forgotten to say that Vdd = 3.3 V

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 02:32 PM
更新者: