2054641_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2054641_en-US

2054641_en-US

SC18IS604 5V tolerant I/O pins

Hello NXP,

I am currently designing a circuit using the SC18IS604. After reading its datasheet, I couldn’t determine which I/O pins are 5V tolerant. I’m sorry to bother you, but I would like to ask the following questions.

1. When the GPIO pins of the SC18IS604 are configured as input-only, are they 5V tolerant?
2. Are the SDA and SCL lines input/output tolerant? If VDD is 3.3V, is it possible to pull up the I2C-bus to 5V?

Best regards,

Yuichiro

Re: SC18IS604 5V tolerant I/O pins

Hello Tomas,

Thank you so much for your quick reply.
I now understand the specifications clearly.

Best regards,
Yuichiro

Re: SC18IS604 5V tolerant I/O pins

Hello Yuichiro,

1. Yes.
2. SCL, SDA pins are not 5V tolerant. These pins should not be pulled up to more than VDD.

BRs, Tomas

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 04:25 PM
更新人: