2051338_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2051338_en-US

2051338_en-US

Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0

I have been trying to install the S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0 in both the new version (S32 DS Version 3.6) as well as the old version (S32 DS Version 3.5 Update 14); despite trying multiple times, the installation fails with an error message.

In the case of S32 DS Version 3.5, the error message is as follows:

Screenshot 2025-02-26 105837.pngScreenshot 2025-02-26 105837.png

 And in the case of S32 DS Version 3.6, it fails with an error message stating that a newer Version of the file has already been installed, but I don't find the file anywhere.

Could someone please help me with this.

Thank you

Re: Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0

Thank you @Robin_Shen for the providing the support!

Re: Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0

It seems that you have installed newer versions of the software packages. You did not follow the instructions to install those versions of the packages. https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K3-RTD-3-0-0-...

Step 6: Remember to select RTD S32K396 for installation


Uninstall and then reinstall the S32DS v3.5 may faster.


The failure of S32DS v3.6 installation may be caused by not running with administrator privileges or IT setting up a firewall.
If you still cannot install S32DS v3.6, it is recommended to create a new question and upload the log file so that our S32DS experts can help you. 
C:\NXP\S32DS.3.6.0\_S32 Design Studio for S32 Platform 3.6.0_installation\Logs


If you still cannot install S32DS v3.6, it is recommended to install S32DS v3.5 + S32K3 RTD 5.0.0 first.

1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe
2. Install Update 13 for S32DS: SW32_S32DS_3.5.13_D2407.zip
3. Install development package for S32K3XX: SW32K3_S32DS_3.5.13_D2407
4. Install development package for S32K396: SW32K39x_S32DS_3.5.13_D2407.zip
5. Install development package for S32M276: SW32M2_S32DS_3.5.13_D2407
6. Install updatesite for this release: SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.
zip
Re: Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0

@Robin_Shen I have gone through the procedure you have suggested and installed the latest version of the software as well as the RTD for the same via offline zip folder, however I am facing an issue with regard to installing/updating the RTD package files in the "S32 DS Extensions and Updates", where the same issue persists as before while installing the RTD package:

Screenshot 2025-02-26 225938.pngScreenshot 2025-02-26 225938.png

 The installation error is reverting to the same issue that a newer version of S32K396 Development Kit is already installed, however any example project with regard to S32K396 is not found in this list:

Screenshot 2025-02-26 225759.pngScreenshot 2025-02-26 225759.png

Could you please help me finding the example projects for S32K396 Evaluation board.

Thank you



Re: Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0

Could you please share the example projects that are visible to you after offline installation

Re: Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0

These examples are provided by S32K3 RTD.
I just installed SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip offline in S32DS v3.6 and I can see these examples. 

SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip can be download by click S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M -> S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 5.0.0

Re: Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0I am actually trying to install the IDE version 3.5 from the link you have provided, but the installer is rolling back.
I am running an example project from the User guide specified for version 3.5, provided by the vendor https://www.nxp.com/document/guide/getting-started-with-s32k396-bga-dc1-evaluation-board:GS-S32K396-... to blink LED 10 times, is there a similar example project in Version 3.6 as well to test if the board is up and running
Re: Installation of S32K396 Development Package and S32K396 RTD AUTOSAR R21-11 Version 3.0.0

Hi

Why do you want to install S32K3 RTD 3.0.0? If you want to import the sample project developed based on this version, please refer to: HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5

It is recommended to install the latest S32K3 RTD 5.0.0 + S32DS v3.5

The S32K3xx Development Package 3.6.0 RFP is installed by default in S32DS v3.6.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:23 PM
Updated by: