2046848_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2046848_en-US

2046848_en-US

Load Error : S32K144 SDK & S32 DS for S32 platform

S32K144EVB  S32DS-S32PLATFORM S32DS-ARM 

Hi, 

I have a trouble when I'm trying to let my S32DS-S32PLATFORM  get the S32K144 SDK. Because I can't find the S32K144 SDK just like S32DS for ARM as the following picture, I download the S32SDK_S32K1xx_RTM_4.0.2.exe and install. 

Endimionchen_1-1739933997772.png

After installing the SDK and choosing sdk_manifest.xml to load,  there is another error: incorrect root tag as the following picture: 

Endimionchen_2-1739934490750.png

Then I try the online updating, it tells me that I have installed the development package as the following picture. But I still can't see the S32K144 SDK appears in the SDK management. 

Endimionchen_3-1739934761359.png


Why S32DS-S32PLATFORM can't load it and how can I fix it and let it load the SDK??

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi Senlent, 


I got it!! I find that it can be chosen by myself just now!! Thanks for your support!!

螢幕擷取畫面 2025-02-21 151625.png

螢幕擷取畫面 2025-02-21 151541.png

 


 

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi@Endimionchen

I mean you need to select GCC 6.3

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi Senlent, 

My GCC version is 10.2. 

螢幕擷取畫面 2025-02-21 150315.png

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi@Endimionchen

I think you chose the wrong version of GCC.

Capture.JPG

 

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi Senlent, 

Yes, I can open and complie the routines by default. The S32K144_SDK has attached on them. 

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi@Endimionchen

I understand your question.
I want you to confirm whether you can open and compile the routines we provide by default.

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi Senlent, 

Thanks for your replay. 

It's right that he Project from Example has attached the S32K144_SDK.

But my demand is to new a project by myself. It seems that in v3.5 still can't let me choose S32K144_SDK even I have installed the both package. Can it be solved??

 

螢幕擷取畫面 2025-02-21 142253.png

  

螢幕擷取畫面 2025-02-21 142728.png

 

 

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi@Endimionchen

Please check below two highlight part have been installed.

Capture.JPG

If all requirements are installed correctly, you can see the examples and the build is

successful.

Capture.JPG

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi senlent, 


I tried v3.5. It could install the SDK, but there were other problems here: 

1. After I install the SDK and the SDK management appeared, I tried to new an Application project. The SDKs still didn't appear the S32K144_SDK to choose as the following picture. 

螢幕擷取畫面 2025-02-20 230633.png

2.  I opened the SDK management. There were S32K144_SDK but there were nothing in it after I check the show attached. 

螢幕擷取畫面 2025-02-20 230718.png

How can I fix it?? 

Re: Load Error : S32K144 SDK & S32 DS for S32 platform

Hi@Endimionchen

Please try to install a version below S32 DS V3.6, such as S32 DS V3.4 and S32 DS V3.5

S32 DS V3.6 should not have pushed the S32K1 SDK package.

In S32 DS V3.4 and S32 DS V3.5, users can see the S32K1 SDK package pushed on this

interface

S32 DS V3.5 Or S32 DS V3.4 with S32K1xx development package installed, you will see S32SDK.

Senlent_0-1739944228863.png


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:30 PM
Updated by: