Hi experts
I'm using BESS_Demo_BmsSL_SAF_V0_8_0. I have installed all the sdk in the dependencies.txt , imported Reference_Application_1500 ,generated code in mex file ,and modified these macros as follow
#define IPCF_IP_CFG_VENDOR_ID_C 43
#define IPCF_IP_CFG_VENDOR_ID 43
When I want to build the porject , I got many erros as below
Then , I found that there is no file in the folder s32k_saf_1_0_4
Is there any problem?
Thanks
Hi
Did you install S32K3_SAF_1.0.4_EVAL_DS_updatesite.zip? (BESS\BESS_2024_06\Safety_Software_Framework_Demo_1_0_4\S32K3_SAF_1.0.4_EVAL_DS_updatesite.zip)
After the installation is complete, you need to modify the Location:
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------